Unary alarm setup parameters

Configure the unary alarm setup parameters as required.

ION Setup controls are shown in parentheses.

Setting Option or range Description
Enable Yes (checked) or No (cleared) This enables or disables the alarm.
Priority High, Medium, Low, None This sets the alarm priority and notification options.

Select Dig Output (Outputs)

Select Relay (Outputs)

None

Digital Output D1

Digital Output D2

Digital Output D1+D2

Relay R1

Relay R2

Relay R1+R2

Select the output(s) you want to control when the alarm is triggered.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?