Viewing alarms counters using the display

Every occurrence of each type of alarm is counted and recorded in the meter.
NOTE: The alarm counters roll over to zero after reaching the value 9999.
  1. Select Alarm > Count .

    The Alarms Counter screen displays.

  2. Scroll through the list to view the number of alarm occurrences for each type of alarm.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?