Configuring the LED for alarms using the display

You can use the meter display to configure the alarm / energy pulsing LED for alarming.
  1. Navigate to the LED setup menu screen.
  2. Set the mode to Alarm, then press OK.
  3. Press the up arrow to exit. Press Yes to save your changes.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?