HMI setup screens

You can configure the meter’s display using the HMI setup screens.

The HMI (human-machine interface) setup screens allow you to:

  • control the general appearance and behavior of the display screens,

  • change the regional settings,

  • change the meter passwords,

  • enable or disable the QR code feature for accessing meter data.

See the Meter Insights QR code feature quick start guide for more information on accessing meter data using QR codes.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.