Default data display screen

The default data display screen varies depending on the meter model.

The Summary screen is the default screen for all meter models except PM5331 / PM5341 .

The Summary screen displays real-time values for average voltage and current (Vavg, Iavg), total power (Ptot) and energy consumption (E Del).

The Power System screen is the default screen for PM5331 / PM5341 meter models.

 

A

Accumulated real energy (delivered + received)

 

B

Active tariff

 

C

System frequency

 

D

Power system setting

 

E

Control power (auxiliary power) interruption event icon

 

F

Locked / unlocked icon

     

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.