Notification icons

To alert you about meter state or events, notification icons appear at the top left or top right corner of the display screen.
Icon Description

The wrench icon indicates that the power meter requires maintenance.

The alarm icon indicates an alarm condition has occurred.

The blinking heartbeat icon indicates that the power meter is in normal operating condition.

(Displayed only in MID/MIR compliance meter models)

The icon indicates that a control power (auxiliary power) interruption event has occurred.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.