Installation
This chapter provides the information required to install the PowerLogic™ DVR system and its associated equipments.
Read and understand all instructions in this manual prior to installation. The correct installation of the PowerLogic™ DVR system is essential for proper operation of all components.
For installation, the location chosen should provide working clearances complying with applicable local standards.
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Follow the steps for the installation of PowerLogic™ DVR system and its associated equipments:
-
Make sure that the foundation is prepared for the PowerLogic™ DVR system. Refer Mounting
. -
Make sure that the environmental requirements are satisfied. Refer Environmental Precautions.
-
Attach the enclosure to the floor.
-
Do the electrical connections for the PowerLogic™ DVR system. Refer Electrical Connections.
-
Set up the parallel interconnections if applicable.
-
Make the remote control wiring connections.
DANGER