NNZ6555100-01

Remote Control from Manual Bypass

The PowerLogic™ DVR master is provided with the terminals to connect to the manual bypass cabinet. Refer to the following image for the location of the terminals. The function of these terminals is to receive the start and stop commands from the manual bypass cabinet. The terminals are located at the bottom of the left door of the PowerLogic™ DVR master only.

The functions of the terminals are:

  • Terminals 1 and 2 – Start-up order (NO): The Start key I4 of the manual bypass closes the contact and starts the PowerLogic™ DVR system.

  • Terminals 3 and 4 – Stop order (NC): The Lock key of the switch I2 of the manual bypass opens the contact and stops the PowerLogic™ DVR system.

The interconnection between manual bypass cabinet and master unit is provided with the cable length of 4.5 m.

Apply tightening torque of 0.5 N⋅m to the screws used for remote control terminals.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?