Recommended Upstream Protection
It is recommended to place an upstream protection that houses only the incoming electrical installation to the equipment. The function of all visible elements in the switchboards shall be clearly indicated.
The upstream connection switchgear consists of:
-
Overcurrent and short-circuit protection: An upstream circuit breaker must be installed at the input of the system according to the recommendations provided in the following table. If the short-circuit current capacity at DVR point connection is greater than the PowerLogic™ DVR short-circuit withstand rating (refer table), use current-limitation circuit breaker.
-
Overvoltage protectors: It is recommended that the general supply connection to the building be fitted with protector against surges due to atmospheric discharges.
-
Differential protection: If a differential protection is used, it should be type B with a minimum time delay of 100 ms, and a minimum value should be set depending on the system configuration.
Master
Master + 1 Slave
Master + 2 Slaves
1 A
2 A
3 A
The following table details the recommended upstream circuit breaker and its settings, and the short-circuit withstand rating of the system.
PowerLogic™ DVR 380/400/415 Vac Systems |
||||||
---|---|---|---|---|---|---|
Maximum sag correction |
PowerLogic™ DVR system power |
Recommended upstream circuit breaker |
Overload settings for upstream circuit breaker |
PowerLogic™ DVR short-circuit rating |
||
Ir |
Tr |
Isd |
||||
-40% |
150 kVA |
ComPact NSX400 MicroLogic 2 |
285 A |
8 s |
10 |
15 kA |
220 KVA |
ComPact NSX630 MicroLogic 2 |
418 A |
8 s |
10 |
15 kA |
|
300 kVA |
ComPact NSX630 MicroLogic 2 |
570 A |
8 s |
10 |
15 kA |
|
440 kVA |
ComPact NS1000 MicroLogic 2 |
836 A |
8 s |
10 |
30 kA |
|
500 kVA |
ComPact NS1000 MicroLogic 2 |
950 A |
8 s |
10 |
30 kA |
|
600 kVA |
ComPact NS1250 MicroLogic 2 |
1140 A |
8 s |
10 |
30 kA |
|
750 kVA |
ComPact NS1600 MicroLogic 2 |
1425 A |
8 s |
10 |
45 kA |
|
900 kVA |
ComPact NS2000 MicroLogic 2 |
1709 A |
8 s |
10 |
45 kA |
|
-50% |
220 kVA |
ComPact NSX630 MicroLogic 2 |
446 A |
8 s |
10 |
12 kA |
440 kVA |
ComPact NS1000 MicroLogic 2 |
891 A |
8 s |
10 |
24 kA |
|
660 kVA |
ComPact NS1600 MicroLogic 2 |
1337 A |
8 s |
10 |
36 kA |
|
-60% |
150 kVA |
ComPact NSX400 MicroLogic 2 |
326 A |
8 s |
10 |
12 kA |
300 kVA |
ComPact NS800 MicroLogic 2 |
651 A |
8 s |
10 |
24 kA |
|
450 kVA |
ComPact NS1000 MicroLogic 2 |
977 A |
8 s |
10 |
36 kA |
PowerLogic™ DVR 200/208/220 Vac Systems |
||||||
---|---|---|---|---|---|---|
Maximum sag correction |
PowerLogic™ DVR system power |
Recommended upstream circuit breaker |
Overload settings for upstream circuit breaker |
PowerLogic™ DVR short-circuit rating |
||
Ir |
Tr |
Isd |
||||
-40% |
150 kVA |
ComPact NSX630 MicroLogic 2 |
541 A |
8 s |
10 |
28 kA |
220 kVA |
ComPact NS800 MicroLogic 2 |
794 A |
8 s |
10 |
28 kA |
|
300 kVA |
ComPact NS1250 MicroLogic 2 |
1083 A |
8 s |
10 |
28 kA |
|
440 kVA |
ComPact NS1600 MicroLogic 2 |
1588 A |
8 s |
10 |
56 kA |
|
500 kVA |
ComPact NS2000 MicroLogic 2 |
1805 A |
8 s |
10 |
56 kA |
|
600 kVA |
ComPact NS2500 MicroLogic 2 |
2165 A |
8 s |
10 |
56 kA |
|
750 kVA |
ComPact NS3200 MicroLogic 2 |
2707 A |
8 s |
10 |
84 kA |
|
900 kVA |
ComPact NS3200 MicroLogic 2 |
3200 A |
8 s |
10 |
84 kA |
|
-50% |
220 kVA |
ComPact NS1000 MicroLogic 2 |
847 A |
8 s |
10 |
22 kA |
440 kVA |
ComPact NS2000 MicroLogic 2 |
1694 A |
8 s |
10 |
44 kA |
|
660 kVA |
ComPact NS3200 MicroLogic 2 |
2540 A |
8 s |
10 |
66 kA |
|
-60% |
150 kVA |
ComPact NSX630 MicroLogic 2 |
619 A |
8 s |
10 |
22 kA |
300 kVA |
ComPact NS1250 MicroLogic 2 |
1237 A |
8 s |
10 |
44 kA |
|
450 kVA |
ComPact NS2000 MicroLogic 2 |
1856 A |
8 s |
10 |
66 kA |