D3349881_00

About the Device

The 5516RVF, 5508RVF, and 5504RVF are new generation C-Bus Voltage Free Relays for general switching of lighting or small motor loads, designed for switchboard distribution applications.

The units are DIN rail mounted, with the 16-channel version measuring 12 modules wide, and the 8 and 4 channel models measuring 8 modules wide (1 module = 18mm).

C-Bus connection is achieved through the use of RJ45 connectors, allowing similar units to be looped together quickly.

Features:

  • DIN Rail mount

  • Integrated Switchable C-Bus Power Supply

  • Latching relays to reduce energy consumption

  • 230 / 110 V nominal voltage

  • Advanced status information for monitoring unit health

  • Warn Before Off function notifying users before lights are turned off for public spaces

  • Configurable Interlock Sets for each channel, enabling priority of operation between channels

  • Logic groups to organize and control relay channels together, flexibly

  • Full configuration with SpaceLogic C-Bus Commission

  • Programming via C-Bus connection without an energized mains line

  • Firmware upgradeable

  • 3 models:

    • 16 channel (5516RVF)

    • 8 channel (5508RVF)

    • 4 channel (5504RVF)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?