D3349881_00

Enable/Disable C-Bus System Clock Generator from the Front Panel

A C-Bus clock signal is required to synchronize communication on the C-Bus Network. The relay unit (and most other C-Bus DIN Rail mounted devices) can be configured to generate the C-Bus system clock.

It is recommended that the C-Bus system clock generator function be enabled in three units on each network segment.

If a C-Bus system clock is required on the relay unit, it can be enabled or disabled from the front panel by performing a short press on the top second-to-right channel button whilst holding down the top left channel button. This toggles the enabled state of the C-Bus system clock generator in the unit.

Once the desired setting for the C-Bus system clock generator, the function to change the setting from the front panel may be disabled via the SpaceLogic C-Bus Commission software to prevent further changes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?