DOCA0271EN-00

Document Scope

This user guide provides:

  • instructions for configuring a TeSys™ island device within the Rockwell Software® Studio 5000® environment.

  • add-on instructions for TeSys island and is valid for use with Studio 5000 environment version 30.0 or greater.

  • add-on instructions, referred to as function blocks for the Studio 5000 environment, control the Avatar and device modules of a TeSys island.

Library Compatibility: L5X files exported from SoMove software are compatible with Studio 5000 major version 30 or higher. Refer to the Product Compatibility and Downloads page on the Rockwell Automation website to verify that the PLC firmware is compatible with the Studio 5000 version being used. As of the time of publication, this information can be found at https://compatibility.rockwellautomation.com.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?