DOCA0271EN-00

List of TeSys Avatars

TeSys Avatars

Name

Icon

Description

System avatar

A required avatar that enables a single point of communication to the TeSys island .

Device

Switch

To make or break a power line in an electrical circuit

Switch - SIL Stop, W. Cat 1/2*

To make or break a power line in an electrical circuit with Stop Category 0 or Stop Category 1* function compliance for Wiring Category 1 and Category 2.

Switch - SIL Stop, W. Cat 3/4*

To make or break a power line in an electrical circuit with Stop Category 0 or Stop Category 1 function compliance for Wiring Category 3 and Category 4.

Digital I/O

To provide control of 2 digital outputs and status of 4 digital inputs

Analog I/O

To provide control of 1 analog output and status of 2 analog inputs

Load

Power Interface without I/O (measure)

To monitor current supplied to an external device, such as a solid-state relay, soft starter, or variable speed drive

Power Interface with I/O (control)

To monitor current supplied to and to control an external device, such as a solid-state relay, soft starter, or variable speed drive

Motor One Direction

To manage* a motor in one direction

Motor One Direction -
SIL Stop, W. Cat 1/2

To manage a motor in one direction, with Stop Category 0 or Stop Category 1 function compliance for Wiring Category 1 and Category 2.

Motor One Direction -
SIL Stop, W. Cat 3/4

To manage a motor in one direction, with Stop Category 0 or Stop Category 1 function compliance for Wiring Category 3 and Category 4.

Motor Two Directions

To manage a motor in two directions (forward and reverse)

Motor Two Directions -
SIL Stop, W. Cat 1/2

To manage a motor in two directions (forward and reverse), with Stop Category 0 or Stop Category 1 function compliance for Wiring Category 1 and Category 2

Motor Two Directions -
SIL Stop, W. Cat 3/4

To manage a motor in two directions (forward and reverse), with Stop Category 0 or Stop Category 1 function compliance for Wiring Category 3 and Category 4

Motor Y/D One Direction

To manage a wye-delta (star-delta) motor in one direction

Motor Y/D Two Directions

To manage a wye-delta (star-delta) motor in two directions (forward and reverse)

Motor Two Speeds

To manage a two-speed motor and two-speed motor with Dahlander option

Motor Two Speeds -
SIL Stop, W. Cat 1/2

To manage a two-speed motor, with Stop Category 0 or Stop Category 1 function compliance for Wiring Category 1 and Category 2

Motor Two Speeds -
SIL Stop, W. Cat 3/4

To manage a two-speed motor, with Stop Category 0 or Stop Category 1 function compliance for Wiring Category 3 and Category 4

Motor Two Speeds Two Directions

To manage a two-speed motor in two directions (forward and reverse)

Motor Two Speeds Two Directions -
SIL Stop, W. Cat 1/2

To manage a two-speed motor in two directions (forward and reverse), with Stop Category 0 or Stop Category 1 function compliance for Wiring Category 1 and Category 2

Motor Two Speeds Two Directions -
SIL Stop, W. Cat 3/4

To manage a two-speed motor in two directions (forward and reverse), with Stop Category 0 or Stop Category 1 function compliance for Wiring Category 3 and Category 4

Resistor

To manage a resistive load

Power Supply

To manage a power supply

Transformer

To manage a transformer

Application

Pump

To manage a pump

Conveyor One Direction

To manage a conveyor in one direction

Conveyor One Direction -
SIL Stop, W. Cat 1/2

To manage a conveyor in one direction, with Stop Category 0 or Stop Category 1 function compliance for Wiring Category 1 and Category 2

Conveyor Two Directions

To manage a conveyor in two directions (forward and reverse)

Conveyor Two Directions -
SIL Stop, W. Cat 1/2

To manage a conveyor in two directions (forward and reverse), with Stop Category 0 or Stop Category 1 function compliance for Wiring Category 1 and Category 2

NOTE: For two speed two direction avatar disable current phase reversal trip.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?