DOCA0224EN-10

Version 003.002.000

New Features

  • Configurable Fallback Mode

    For starters and IO module outputs, the fallback position can be configured for each avatar except Power Interface avatar.

  • Korean language support

    Korean language is supported in SoMove and Operation and Maintenance Tool (OMT).

  • Avatar trip status for IO PORT ASSIGNMENT

    IO PORT ASSIGNMENT table lists avatar trip status and individual trip status, which can be assigned to digital outputs.

  • Configurable communication loss time-out for Fieldbus Protocol

    Communication loss time-out can be configured for the Fieldbus Protocol.

Bugs Fixed

Positive Temperature Coefficient (PTC) Binary as Process Variable (PV) input.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.