DOCA0224EN-10

Compatibility

@Updated D1

The following table shows the compatibility of digital tools with TeSys island module in active releases.

Configuration/Programming software

TeSys island firmware version

TeSysisland_001.100.0013.sedp

TeSysisland_002.100.016.sedp

TeSysisland_002.200.008.sedp

TeSysisland_002.300.006.sedp

TeSysisland_003.000.002.sedp

TeSysisland_003.001.001.sedp

TeSysisland_003.002.000.sedp

TeSysisland_003.003.000.sedp

TeSysisland_003.003.001.sedp

TeSysisland_003.003.005.sedp

DTM (SoMove or any FDT container)

DTM v1.0.1401

X

X

X

X

X

X

X

X

X

DTM v1.1.0

X

X

X

X

X

X

X

X

X

DTM v2.1.1

X

X

X

X

X

X

X

X

NOTE: DTM v2.1.1 is compatible when using Modbus TCP or EtherNet/IP and for previously existing device and load avatars only.
 

DTM v2.2.0 or DTM v2.2.1 (equivalent)

X

X

X

X

X

X

X

X

DTM v2.3.0

X

X

X

X

X

X

X

X

X

DTM v2.4.0

X

X

X

X

X

X

X

X

X

X

DTM v2.4.1

X

X

X

X

X

X

X

X

DTM v2.4.2

X

X

X

X

X

X

X

X

X

DTM v2.4.3

X

X

X

X

X

X

X

X

X

DTM v2.4.4

X

X

X

X

X

X

X

X

X

DTM v3.0.0

X

X

X

X

X

X

X

X

DTM v3.0.1

X

X

X

X

X

X

X

X

DTM v3.0.2

X

X

X

X

X

X

X

X

X

EcoStruxure Machine Expert

EcoStruxure Machine Expert v1.1 or v1.2

Function block library: 1.0.15.0

Device description:

  • Modbus TCP: 1.1.0.0

  • Ethernet/IP: 1.1.0.0

X

X

X

X

X

X

X

X

X

EcoStruxure Machine Expert v1.2.3 or later

Function block library: 2.0.2.0

Device description:

  • Modbus TCP: 1.1.6

  • Ethernet/IP: 1.1.7

X

X

**

**

X

X

X

X

EcoStruxure Machine Expert v2.2.2

Function block library: 3.0.0.0

Device description:

  • Modbus TCP: 1.0.1.0

  • Ethernet/IP: 1.0.2.11

X

X

X

X

X

X

*

X

X

X

EcoStruxure Machine Expert v2.3

Function block library: 4.0.6.0

Device description:

  • Modbus TCP: 1.0.1.0

  • Ethernet/IP: 1.0.2.11

X

X

X

X

X

X

X

X

***

NOTE:
  1. *If the default IO port assignment is changed or local control is used for safe category avatars, then the function blocks in EcoStruxure Machine Expert are not compatible.

  2. **Function blocks library for PLCs with Machine Expert on Modbus TCP protocol is not compatible.

  3. ***All new parameters (ATEX configuration status and minor event status for all avatars) will be not be available in Control Function Blocks.

Workaround: Use the Schneider Electric Machine Expert Modbus TCP PLCs as a third party PLC.

EcoStruxure Automation Expert-Motion

EcoStruxure Automation Expert-Motion vM_24.1.0.0

Function block library: 4.0.5.0

Device description:

  • Modbus TCP: 1.0.1.0

  • Ethernet/IP: 1.0.2.11

X

X

X

X

X

X

X

*

NOTE: *All new parameters (ATEX configuration status and minor event status for all avatars) will be not be available in Control Function Blocks.

EcoStruxure Control Expert V15.0 SP1

EcoStruxure Control Expert–TeSys island Library

PSx DTM Library v3.14.54

PLC M580 - CPU firmware 3.20

X

X

*

*

*

X

X

X

NOTE: *EcoStruxure Control Expert is not compatible, if there is change in the IO PORT ASSIGNMENT.

EcoStruxure Control Expert V16.0 or later

EcoStruxure Control Expert–TeSys island Library v2.2

PSx DTM Library v3.19.24107

PLC M580 - CPU firmware 3.20

X

X

X

X

X

X

X

*

NOTE: *All new parameters (ATEX configuration status and minor event status for all avatars) will be not be available in Control Function Blocks.

Studio 5000 V30 or later

NA

NA

NA

*

*

*

X

X

X

NOTE: Ensure that the export of L5X file is done with the compatible version of DTM.
NOTE: *When PIM with IO avatar is used with TeSys island, then the function blocks are not compatible with RS5000.

TIA Portal V15 or later

Library: TeSysisland_TIAV15_V2.1.1.zal15

GSD: SCHE1135.GSD (revision 1.0)

GSDML: GSDML-V2.35-SchneiderElectric-TeSysisland-20200202.xml

NOTE: Ensure that the export of AML file is done with the compatible version of DTM.

X

X

X

X

X

X

X

X

X

Library: TeSysIsland_TIAV15_V2.2.0.zal15

GSD: SCHE1135.GSD (revision 2.0)

GSDML: GSDML-V2.35-SchneiderElectric-TeSysisland-20200404.xml

NOTE: Ensure that the export of AML file is done with the compatible version of DTM.

X

X

*

*

*

X

X

X

NOTE: *When PIM with IO avatar is used with TeSys island, then the function blocks are not compatible with TIA portal.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?