DOCA0224EN-10

Firmware Release History

The following table provides the summary of each TeSys island firmware package and bus coupler version:

Date

SEDP package version

Bus coupler version

Notes

January 2026

TeSys island_003.003.005.sedp

003.003.005

Following features are updated:

  • Limit the device minor events to Avatar.

  • Adapt TeSys island for ATEX application.

June 2025

TeSys island_003.003.001.sedp

003.003.001

IO Optimization feature extension to EcoStruxure Machine Expert function blocks library.

April 2025

TeSys island_003.003.000.sedp

003.003.000

IO Optimization feature extension to EcoStruxure Automation Expert-Motion function blocks library.

December 2024

TeSys island_003.003.000.sedp

003.003.000

IO Optimization feature extension to EcoStruxure Control Expert function blocks library.

April 2024

TeSys island_003.002.000.sedp

003.002.000

Following features are updated:

  • Configurable Fallback Mode

  • Korean language support

  • Avatar trip status for IO PORT ASSIGNMENT

  • Configurable communication loss timeout for Fieldbus Protocol

August 2023

TeSys island_003.001.001.sedp

003.001.001

Korean language support.

June 2023

TeSys island_003.000.002.sedp

003.000.002

Power Interface with IO avatar is enabled for IO Optimization.

February 2023

TeSys island_003.000.001.sedp

003.000.001

Following features are updated:

  • IO Optimization

  • Local control for safe category avatars

  • Local Trip Reset for individual avatars

September 2021

TeSys island_002.300.006.sedp

002.300

Release with Dahlander and few security improvements.

May 2020

TeSys island_002.200.008.sedp

02.0200

Release with extended local control modes and their integration into EcoStruxure Machine Expert software.

February 2020

TeSys island_002.100.016.sedp

02.0100

Patch of firmware version 2.1.0.13 with Achilles certification.

January 2020

TeSys island_002.100.013.sedp

02.0100

Release of PROFINET and PROFIBUS-DP communication and new avatars. The firmware version is not compatible with EcoStruxure Machine Expert library.

June 2019

TeSys island_001.100.013.sedp

01.0100

Initial release

Bus Coupler Firmware

The bus coupler firmware can be updated on the following TeSys island bus couplers:

  • TPRBCEIP (Ethernet/IP or Modbus TCP)

  • TPRBCPFN (PROFINET)

  • TPRBCPFB (PROFIBUS-DP)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?