DOCA0130EN-03

TCC

trip curve characteristic. The type of delay used to trip the flow of current in response to a trip condition. As implemented in the LTMR controller, all motor protection function trip time delays are definite time, except for the Thermal Overload function, which also offers inverse thermal trip time delays.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?