DOCA0130EN-03

TVC

trip voltage characteristic. The type of delay used to trip the flow of voltage in response to a trip condition. As implemented by the LTMR controller and the expansion module, all TVCs are definite time.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?