Using the Modbus Communication Network
Overview
This chapter describes how to use the LTMR controller via the network port using the Modbus protocol.
WARNING |
|---|
|
LOSS OF CONTROL
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
(1) For additional information, refer to NEMA ICS 1.1 (latest edition), "Safety Guidelines for the Application, Installation, and Maintenance of Solid State Control".
WARNING |
|---|
|
UNEXPECTED RESTART OF THE MOTOR
Check that the PLC application software:
When switching to the Network control channels,
depending on the communication protocol configuration, the LTMR controller can take into account the latest
known state of the motor control commands issued from the PLC and
restart automatically the motor.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Modbus Protocol Principle
Overview
Only one device can transmit on the line at any time.
The primary device manages and initiates the exchange. It interrogates each of the secondary devices in succession. No secondary device can send a message unless it is invited to do so.
The primary device repeats the question when there is an incorrect exchange, and declares the interrogated secondary device absent if no response is received within a given time period.
If a secondary device does not understand a message, it sends an exception response to the primary device. The primary device may or may not retransmit the request.
Modbus Dialog
Two types of dialog are possible between primary and secondary devices:
-
The primary device sends a request to a secondary device and waits for its response.
-
The primary device broadcasts a request to all secondary devices without waiting for a response.
Direct secondary-to-secondary communication is not possible. For secondary-to-secondary communication, the primary device must interrogate a secondary device and send back data received to the other secondary device.
Transparent Ready
The controller LTMR Modbus is of class A05 (Transparent Ready).
Configuration of the LTMR Modbus Network Port
Communication Parameters
Before any communication can start, use the TeSys T DTM or the HMI to configure the Modbus port communication parameters:
-
Network port address setting
-
Network port baud rate setting
-
Network port parity setting
-
Network port comm loss timeout
-
Network port endian setting
Network Port Address Setting
The device address can be set between 1 and 247.
Factory setting is 1, which corresponds to an undefined value.
Network Port Baud Rate Setting
Possible transmission rates are:
-
1200 Baud
-
2400 Baud
-
4800 Baud
-
9600 Baud
-
19,200 Baud
-
Autodetection
Factory settings is Autodetection. In Autodetection, the controller is able to adapt its baud rate to that of the primary device. 19,200 Baud is the first baud rate to be tested.
Network Port Parity Setting
The parity can be selected from:
-
Even
-
Odd
-
None
When Network port baud rate setting is in Autodetection, the controller is able to adapt its parity and stop bit to that of the primary device. Even parity is the first parity to be tested.
In Autodetection, the parity is set automatically; any previous setting is ignored.
Parity and stop bit behavior is linked:
|
If the Parity Is... |
Then the Number of Stop Bits Is... |
|---|---|
|
even or odd |
1 |
|
none |
2 |
Network Port Comm Loss Timeout
Network port comm loss timeout is used to determine the timeout value after a loss of communication with the PLC.
-
Range: 1-9,999
Network Port Fallback Setting
Network port fallback setting is used to adjust the fallback mode in case of a loss of communication with the PLC.
Network Port Endian Setting
The Network port endian setting allows to swap the two words in a double word.
-
0 = least significant word first (little endian)
-
1 = most significant word first (big endian, factory setting)
Modbus Communication Checking
Introduction
Configure the networking function last. Even when the connectors are plugged in, communication between the controller(s) and the PLC cannot start until you enter the correct communication parameters via SoMove with the TeSys T DTM or the HMI.
You can then check whether your system can communicate properly.
Step 1
On the LTMR front face, check the following two LEDs:
-
Fallback
-
PLC Comm
The communication Fallback is indicated by a red LED (1).
|
If the red Fallback LED is... |
Then... |
|---|---|
|
OFF |
the LTMR is not in communication fallback mode |
|
ON |
the LTMR is in communication fallback mode |
The Modbus communication status, marked as PLC Comm, is indicated by a yellow LED (2).
|
If the yellow PLC Comm LED is... |
Then... |
|---|---|
|
OFF |
the LTMR is not communicating |
|
Blinking |
the LTMR is exchanging frames (receiving or sending) |
Step 2
If the product should be communicating but the LEDs are not lit, check the cables and connectors and correct any connection problems.
Step 3
If the product is still not communicating, check the configuration via:
-
SoMove with the TeSys T DTM, or
-
The HMI.
The detected communication interruption can be the result of a wrong address, speed or parity; or an incorrect PLC configuration.
Simplified Control and Monitoring
Modbus Request and Programming Examples
Modbus Request
The following table indicates which Modbus functions are managed by the LTMR controller, and specifies their limits:
|
Code value |
Function Name |
Broadcasting |
Modbus Standard Name |
|
|---|---|---|---|---|
|
Hexadecimal |
Decimal |
|||
|
0x03 |
3 |
Read N output words (multiple registers) |
No |
Read Holding Register |
|
0x06 |
6 |
Write 1 output word (single register) |
Yes |
Preset Single Register |
|
0x10 |
16 |
Write N output words (multiple registers) |
Yes |
Preset Multiple Registers |
|
0x2B |
43 |
Read identification (identification register) |
No |
Read Device Identification |
The maximum number of registers per request is limited to 100.
WARNING |
|---|
|
UNINTENDED EQUIPMENT OPERATION
Use of this device on a Modbus network that uses the broadcast function should be considered with
caution.
This device has a large number of registers that must
not be modified during normal operation. Unintended writing of these
registers by the broadcast function may cause unexpected and unwanted
product operation.
For more information, refer to the Communication variables
list.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Example of a Read Operation (Modbus Request Code 3)
The following example describes a READ_VAR request, within a TSX Micro or Premium platform, in order to read the LTMR states at address 4 (secondary device n° 4) contained in internal word MW0:
1 Address of the device with which you wish to communicate: 3 (device address), 0 (channel), 4 (device address on the bus)
2 Type of PL7 objects to be read: MW (internal word)
3 Address of the first register to be read: 455
4 Number of consecutive registers to be read: 1
5 Word table containing the value of the objects read: MW0:1
6 Read report: MW100:4
Example of a Write Operation (Modbus Request Code 16)
The following example describes a WRITE_VAR request, within a TSX Micro or Premium platform, in order to control an LTMR by sending the contents of internal word MW 502:
1 Address of the device with which you wish to communicate: 3 (device address), 0 (channel), 4 (device address on the bus)
2 Type of PL7 objects to be written: MW (internal word)
3 Address of the first register to be written: 704
4 Number of consecutive registers to be written: 1
5 Word table containing the value of the objects to be sent: MW502:1
6 Write report: MW200:4
Modbus Exception Management
Overview
The LTMR controller generally follows the Modbus requirements for the Exception Management.
Three special cases apply to the LTMR controller:
-
Bit-Field Registers
-
Exception Code 02 - Illegal Data Address
-
Exception Code 03 - Illegal Data Value
Bit-Field Registers
Some registers in the Register Map are bit-field. Based on the LTMR controller state, some bits in those registers shall not be writable. In this case, the LTMR controller shall reject the write to those bits meaning that no exception shall be returned. For example, bits that can be written only in configuration mode will be ignored (no exception returned) if the LTMR controller is out of the Sys Config State. The write to the bits not constrained by the LTMR controller state shall however occur.
Exception Code 02 - Illegal Data Address
In general, the LTMR controller shall return an illegal data address exception code, if the address is out of range or inaccessible. Specifically, the LTMR controller shall return an illegal data address if:
-
A Write request is sent to a Read only register.
-
The permission to write a register is not granted because of the LTMR controller state: this is the case, for example, when a register that can be written only in configuration mode is written while the LTMR controller is out of Sys Config state.
Exception Code 03 - Illegal Data Value
In general, the LTMR controller shall return an illegal data value exception code if there is a problem with the structure of the message, such as an invalid length. The LTMR controller shall also use this exception code if:
-
The data to be written is out of range (for standard and bit-field registers): this is the case if a write request of 100 is sent to a R/W register with a range of 0 to 50.
-
A reserved bit or register is written to a value different than 0.
-
Motor low speed command (bit 704.6) is set while the motor controller mode selected is not a two-speed mode of operation.
User Map Variables (User Defined Indirect Registers)
Overview
User Map variables are designed to optimize the access to several non-contiguous registers in one single request.
You can define several read and write areas.
The user map can be defined via:
-
A PC running SoMove with TeSys T DTM
-
A PLC via the network port
User Map Variables
User Map variables are divided into two groups:
|
User Map Addresses |
800 to 898 |
|
User Map Values |
900 to 998 |
The User Map Address group is used to select a list of addresses to read or write. It can be considered as a configuration area.
The User Map Value group is used to read or write values associated to addresses configured in the User Map Address area:
-
Read or write of register 900 allows to read or write the register address defined in register 800
-
Read or write of register 901 allows to read or write the register address defined in register 801,...
Example of Use
The following table gives an example of user map address configuration to access non-contiguous registers:
|
User Map Address Register |
Value Configured |
Register |
|---|---|---|
|
800 |
452 |
Trip register 1 |
|
801 |
453 |
Trip register 2 |
|
802 |
461 |
Alarm register 1 |
|
803 |
462 |
Alarm register 2 |
|
804 |
450 |
Minimum wait time |
|
805 |
500 |
Average current (0.01 A) MSW |
|
806 |
501 |
Average current (0.01 A) LSW |
|
850 |
651 |
HMI display items register 1 |
|
851 |
654 |
HMI display items register 2 |
|
852 |
705 |
Control register 2 |
With this configuration, monitoring information is accessible with one single read request through register addresses 900 to 906.
Configuration and command can be written with one single write using registers 950 to 952.
Register Map (Organization of Communication Variables)
Introduction
Communication variables are listed in tables, according to the group (such as identification, statistics, or monitoring) to which they belong. They are associated with an LTMR controller, which may or may not have an LTME expansion module attached.
Communication Variable Groups
Communication variables are grouped according to the following criteria:
|
Variable Groups |
Registers |
|---|---|
|
Identification variables |
00 to 99 |
|
Statistics variables |
100 to 449 |
|
Monitoring variables |
450 to 539 |
|
Configuration variables |
540 to 699 |
|
Command variables |
700 to 799 |
|
User Map variables |
800 to 999 |
|
Custom Logic variables |
1200 to 1399 |
Table Structure
Communication variables are listed in 4-column tables:
|
Column 1 Register (in decimal format) |
Column 2 Variable type |
Column 3 Variable name and access via Read-only or Read/Write Modbus requests |
Column 4 Note: code for additional information |
Note
The Note column gives a code for additional information.
Variables without a code are available for all hardware configurations, and without functional restrictions.
The code can be:
-
numerical (1 to 9), for specific hardware combinations
-
alphabetical (A to Z), for specific system behaviors.
|
If the Note Is... |
Then the Variable Is... |
|---|---|
|
1 |
Available for the LTMR + LTMEV40 combination |
|
2 |
Always available but with a value equal to 0 if no LTMEV40 is connected |
|
3 - 9 |
Not used |
|
If the Note Is... |
Then... |
|---|---|
|
A |
The variable can be written only when the motor is off.* |
|
B |
The variable can be written only in configuration mode (e.g. static characteristics).* |
|
C |
The variable can be written only with no trip.* |
|
D - Z |
Not used |
Unused Addresses
Unused addresses fall into three categories:
-
Not significant, in Read-only tables, means that you should ignore the value read, whether equal to 0 or not.
-
Reserved, in Read/Write tables, means that you must write 0 in these variables.
-
Forbidden, means that read or write requests are rejected, that these addresses are not accessible.
Data Formats
Overview
The data format of a communication variable can be integer, Word, or Word[n], as described below. For more information about a variable size and format, refer to Data Types.
Integer (Int, UInt, DInt, IDInt)
Integers fall into the following categories:
-
Int: signed integer using one register (16 bits)
-
UInt: unsigned integer using one register (16 bits)
-
DInt: signed double integer using 2 registers (32 bits)
-
UDInt: unsigned double integer using 2 registers (32 bits)
For all integer-type variables, the variable name is completed with its unit or format, if necessary.
Example:
Address 474, UInt, Frequency (x 0.01 Hz).
Word
Word: Set of 16 bits, where each bit or group of bits represents command, monitoring or configuration data.
Example:
Address 455, Word, System Status Register 1.
|
bit 0 |
System ready |
|
bit 1 |
System on |
|
bit 2 |
System trip |
|
bit 3 |
System alarm |
|
bit 4 |
System tripped |
|
bit 5 |
Trip reset authorized |
|
bit 6 |
(Not significant) |
|
bit 7 |
Motor running |
|
bits 8-13 |
Motor average current ratio |
|
bit 14 |
In remote |
|
bit 15 |
Motor starting (in progress) |
Word[n]
Word[n]: Data encoded on contiguous registers.
Examples:
Addresses 64 to 69, Word[6], Controller Commercial Reference (DT_CommercialReference).
Addresses 655 to 658, Word[4], (DT_DateTime).
Data Types
Overview
Data types are specific variable formats which are used to complement the description of internal formats (for instance, in case of a structure or of an enumeration). The generic format of data types is DT_xxx.
List of Data Types
Here is the list of the most commonly used data types:
-
DT_ACInputSetting
-
DT_CommercialReference
-
DT_DateTime
-
DT_ExtBaudRate
-
DT_ExtParity
-
DT_TripCode
Change Fault to Trip here, or leave as is? -
DT_FirmwareVersion
-
DT_Language5
-
DT_OutputFallbackStrategy
-
DT_PhaseNumber
-
DT_ResetMode
-
DT_AlarmCode
These data types are described below.
DT_ACInputSetting
DT_ACInputSetting format is an enumeration that improves AC input detection:
|
Value |
Description |
|---|---|
|
0 |
None (factory setting) |
|
1 |
< 170 V 50 Hz |
|
2 |
< 170 V 60 Hz |
|
3 |
> 170 V 50 Hz |
|
4 |
> 170 V 60 Hz |
DT_CommercialReference
DT_CommercialReference format is Word[6] and indicates a Commercial Reference:
|
Register |
MSB |
LSB |
|---|---|---|
|
Register N |
character 1 |
character 2 |
|
Register N+1 |
character 3 |
character 4 |
|
Register N+2 |
character 5 |
character 6 |
|
Register N+3 |
character 7 |
character 8 |
|
Register N+4 |
character 9 |
character 10 |
|
Register N+5 |
character 11 |
character 12 |
Example:
Addresses 64 to 69, Word[6], Controller Commercial Reference.
If Controller Commercial Reference = LTMR:
|
Register |
MSB |
LSB |
|---|---|---|
|
64 |
L |
T |
|
65 |
M |
(space) |
|
66 |
R |
|
|
67 |
|
|
|
68 |
|
|
|
69 |
|
|
DT_DateTime
DT_DateTime format is Word[4] and indicates Date and Time:
|
Register |
Bits 12-15 |
Bits 8-11 |
Bits 4-7 |
Bits 0-3 |
|---|---|---|---|---|
|
Register N |
S |
S |
0 |
0 |
|
Register N+1 |
H |
H |
m |
m |
|
Register N+2 |
M |
M |
D |
D |
|
Register N+3 |
Y |
Y |
Y |
Y |
Where:
-
S = second
The format is 2 BCD digits.
The value range is [00-59] in BCD.
-
0 = unused
-
H = hour
The format is 2 BCD digits.
The value range is [00-23] in BCD.
-
m = minute
The format is 2 BCD digits.
The value range is [00-59] in BCD.
-
M = month
The format is 2 BCD digits.
The value range is [01-12] in BCD.
-
D = day
The format is 2 BCD digits.
The value range is (in BCD):
[01-31] for months 01, 03, 05, 07, 08, 10, 12
[01-30] for months 04, 06, 09, 11
[01-29] for month 02 in a leap year
[01-28] for month 02 in a non-leap year.
-
Y = year
The format is 4 Binary Coded Decimal (BCD) digits.
The value range is [2006-2099] in BCD.
Data entry format and value range are:
|
Data Entry Format |
DT#YYYY-MM-DD-HH:mm:ss |
|
|---|---|---|
|
Minimum value |
DT#2006-01-01:00:00:00 |
January 1, 2006 |
|
Maximum value |
DT#2099-12-31-23:59:59 |
December 31, 2099 |
|
Note: If you give values outside the limits, the system will return a detected error. |
||
Example:
Addresses 655 to 658, Word[4], Date and Time setting.
If date is September 4, 2008 at 7 a.m., 50 minutes and 32 seconds:
|
Register |
15 12 |
11 8 |
7 4 |
3 0 |
|---|---|---|---|---|
|
655 |
3 |
2 |
0 |
0 |
|
656 |
0 |
7 |
5 |
0 |
|
657 |
0 |
9 |
0 |
4 |
|
658 |
2 |
0 |
0 |
8 |
With data entry format: DT#2008-09-04-07:50:32.
DT_ExtBaudRate
DT_ExtbaudRate depends on the bus used:
DT_ModbusExtBaudRate format is an enumeration of possible baud rates with Modbus network:
|
Value |
Description |
|---|---|
|
1200 |
1200 Baud |
|
2400 |
2400 Baud |
|
4800 |
4800 Baud |
|
9600 |
9600 Baud |
|
19200 |
19,200 Baud |
|
65535 |
Autodetection (factory setting) |
DT_ProfibusExtBaudRate format is an enumeration of possible baud rates with PROFIBUS DP network:
|
Value |
Description |
|---|---|
|
65535 |
Autobaud (factory setting) |
DT_DeviceNetExtBaudRate format is an enumeration of possible baud rates with DeviceNet network:
|
Value |
Description |
|---|---|
|
0 |
125 kBaud |
|
1 |
250 kBaud |
|
2 |
500 kBaud |
|
3 |
Autobaud (factory setting) |
DT_CANopenExtBaudRate format is an enumeration of possible baud rates with CANopen network:
|
Value |
Description |
|---|---|
|
0 |
10 kBaud |
|
1 |
20 kBaud |
|
2 |
50 kBaud |
|
3 |
125 kBaud |
|
4 |
250 kBaud (factory setting) |
|
5 |
500 kBaud |
|
6 |
800 kBaud |
|
7 |
1000 kBaud |
|
8 |
Autobaud |
|
9 |
Factory setting |
DT_ExtParity
DT_ExtParity depends on the bus used:
DT_ModbusExtParity format is an enumeration of possible parities with Modbus network:
|
Value |
Description |
|---|---|
|
0 |
None |
|
1 |
Even |
|
2 |
Odd |
DT_TripCode
DT_TripCode format is an enumeration of trip codes:
|
Trip Code |
Description |
|---|---|
|
0 |
No detected error |
|
3 |
Ground current |
|
4 |
Thermal overload |
|
5 |
Long start |
|
6 |
Jam |
|
7 |
Current phase imbalance |
|
8 |
Undercurrent |
|
10 |
Test |
|
11 |
Detected HMI port error |
|
12 |
HMI port communication loss |
|
13 |
Detected HMI network port internal error |
|
16 |
External trip |
|
18 |
On-Off diagnostic |
|
19 |
Wiring diagnostic |
|
20 |
Overcurrent |
|
21 |
Current phase loss |
|
22 |
Current phase reversal |
|
23 |
Motor temp sensor |
|
24 |
Voltage phase imbalance |
|
25 |
Voltage phase loss |
|
26 |
Voltage phase reversal |
|
27 |
Undervoltage |
|
28 |
Overvoltage |
|
29 |
Underpower |
|
30 |
Overpower |
|
31 |
Under power factor |
|
32 |
Over power factor |
|
33 |
LTME configuration |
|
34 |
Temperature sensor short-circuit |
|
35 |
Temperature sensor open-circuit |
|
36 |
CT reversal |
|
37 |
Out of boundary CT ratio |
|
46 |
Start check |
|
47 |
Run checkback |
|
48 |
Stop check |
|
49 |
Stop checkback |
|
51 |
Detected controller internal temperature error |
|
55 |
Detected controller internal error (Stack overflow) |
|
56 |
Detected controller internal error (RAM error) |
|
57 |
Detected controller internal error (RAM checksum error) |
|
58 |
Detected controller internal error (Hardware watchdog trip) |
|
60 |
L2 current detected in single-phase mode |
|
64 |
Detected non volatile memory error |
|
65 |
Detected expansion module communication error |
|
66 |
Stuck reset button |
|
67 |
Detected logic function error |
|
100-104 |
Detected network port internal error |
|
109 |
Detected network port comm error |
|
111 |
Fast device replacement trip |
|
555 |
Detected network port configuration error |
DT_FirmwareVersion
DT_FirmwareVersion format is an XY000 array that describes a firmware revision:
-
X = major revision
-
Y = minor revision.
Example:
Address 76, UInt, Controller firmware version.
DT_Language5
DT_Language5 format is an enumeration used for language display:
|
Language Code |
Description |
|---|---|
|
1 |
English (factory setting) |
|
2 |
Français |
|
4 |
Español |
|
8 |
Deutsch |
|
16 |
Italiano |
Example:
Address 650, Word, HMI language.
DT_OutputFallbackStrategy
DT_OutputFallbackStrategy format is an enumeration of motor output states when loosing communication.
|
Value |
Description |
Motor Modes |
|---|---|---|
|
0 |
Hold LO1 LO2 |
For all modes |
|
1 |
Run |
For 2-step mode only |
|
2 |
LO1, LO2 Off |
For all modes |
|
3 |
LO1, LO2 On |
Only for overload, independent and custom operating modes |
|
4 |
LO1 On |
For all modes except 2-step |
|
5 |
LO2 On |
For all modes except 2-step |
DT_PhaseNumber
DT_PhaseNumber format is an enumeration, with only 1 bit activated:
|
Value |
Description |
|---|---|
|
1 |
1 phase |
|
2 |
3 phases |
DT_ResetMode
DT_ResetMode format is an enumeration of possible modes for thermal trip reset:
|
Value |
Description |
|---|---|
|
1 |
Manual or HMI |
|
2 |
Remote by network |
|
4 |
Automatic |
DT_AlarmCode
DT_AlarmCode format is an enumeration of alarm codes:
|
Alarm Code |
Description |
|---|---|
|
0 |
No alarm |
|
3 |
Ground current |
|
4 |
Thermal overload |
|
5 |
Long start |
|
6 |
Jam |
|
7 |
Current phase imbalance |
|
8 |
Undercurrent |
|
10 |
HMI port |
|
11 |
LTMR internal temperature |
|
18 |
Diagnostic |
|
19 |
Wiring |
|
20 |
Overcurrent |
|
21 |
Current phase loss |
|
23 |
Motor temp sensor |
|
24 |
Voltage phase imbalance |
|
25 |
Voltage phase loss |
|
27 |
Undervoltage |
|
28 |
Overvoltage |
|
29 |
Underpower |
|
30 |
Overpower |
|
31 |
Under power factor |
|
32 |
Over power factor |
|
33 |
LTME configuration |
|
46 |
Start check |
|
47 |
Run checkback |
|
48 |
Stop check |
|
49 |
Stop checkback |
|
109 |
Network port comm loss |
|
555 |
Network port configuration |
Identification Variables
Identification Variables
Identification variables are described in the following table:
|
Register |
Variable Type |
Read-only Variables |
|
|---|---|---|---|
|
0-34 |
(Not significant) |
||
|
35-40 |
Word[6] |
Expansion commercial reference (See DT_CommercialReference) |
1 |
|
41-45 |
Word[5] |
Expansion serial number |
1 |
|
46 |
UInt |
Expansion ID code |
|
|
47 |
UInt |
Expansion firmware version (See DT_FirmwareVersion) |
1 |
|
48 |
UInt |
Expansion compatibility code |
1 |
|
49-60 |
(Not significant) |
||
|
61 |
Ulnt |
Network port ID code |
|
|
62 |
Ulnt |
Network port firmware version (See DT_FirmwareVersion) |
|
|
63 |
Ulnt |
Network port compatibility code |
|
|
64-69 |
Word[6] |
Controller commercial reference (See DT_CommercialReference) |
|
|
70-74 |
Word[5] |
Controller serial number |
|
|
75 |
Ulnt |
Controller ID code |
|
|
76 |
Ulnt |
Controller firmware version (See DT_FirmwareVersion) |
|
|
77 |
Ulnt |
Controller compatibility code |
|
|
78 |
Ulnt |
Current scale ratio (0.1 %) |
|
|
79 |
Ulnt |
Current sensor max |
|
|
80 |
(Not significant) |
|
|
|
81 |
Ulnt |
Current range max (x 0.1 A) |
|
|
82-94 |
(Not significant) |
||
|
95 |
Ulnt |
Load CT ratio (x 0.1 A) |
|
|
96 |
Ulnt |
Full load current max (maximum FLC range, FLC = Full Load Current) (x 0.1 A) |
|
|
97-99 |
(Forbidden) |
Statistics Variables
Statistics Overview
Statistics variables are grouped according to the following criteria. Trip statistics are contained into a main table and an extension table.
|
Statistics variable groups |
Registers |
|---|---|
|
Global statistics |
100 to 121 |
|
LTM monitoring statistics |
122 to 149 |
|
Last trip statistics and extension |
150 to 179 300 to 309 |
|
Trip n-1 statistics and extension |
180 to 209 330 to 339 |
|
Trip n-2 statistics and extension |
210 to 239 360 to 369 |
|
Trip n-3 statistics and extension |
240 to 269 390 to 399 |
|
Trip n-4 statistics and extension |
270 to 299 420 to 429 |
Global Statistics
The global statistics are described in the following table:
|
Register |
Variable Type |
Read-only Variables |
|
|---|---|---|---|
|
100-101 |
(Not significant) |
||
|
102 |
Ulnt |
Ground current trips count |
|
|
103 |
Ulnt |
Thermal overload trips count |
|
|
104 |
Ulnt |
Long start trips count |
|
|
105 |
Ulnt |
Jam trips count |
|
|
106 |
Ulnt |
Current phase imbalance trips count |
|
|
107 |
Ulnt |
Undercurrent trips count |
|
|
109 |
Ulnt |
HMI port trips count |
|
|
110 |
Ulnt |
Controller internal trips count |
|
|
111 |
Ulnt |
Internal port trips count |
|
|
112 |
Ulnt |
(Not significant) |
|
|
113 |
Ulnt |
Network port config trips count |
|
|
114 |
Ulnt |
Network port trips count |
|
|
115 |
Ulnt |
Auto-resets count |
|
|
116 |
Ulnt |
Thermal overload alarms count |
|
|
117-118 |
UDlnt |
Motor starts count |
|
|
119-120 |
UDlnt |
Operating time (s) |
|
|
121 |
lnt |
Controller internal temperature max (°C) |
LTM Monitoring Statistics
The LTM monitoring statistics are described in the following table:
|
Register |
Variable Type |
Read-only Variables |
|
|---|---|---|---|
|
122 |
Ulnt |
Trips count |
|
|
123 |
Ulnt |
Alarms count |
|
|
124-125 |
UDlnt |
Motor LO1 closings count |
|
|
126-127 |
UDlnt |
Motor LO2 closings count |
|
|
128 |
Ulnt |
Diagnostic trips count |
|
|
129 |
Ulnt |
(Reserved) |
|
|
130 |
Ulnt |
Overcurrent trips count |
|
|
131 |
Ulnt |
Current phase loss trips count |
|
|
132 |
Ulnt |
Motor temperature sensor trips count |
|
|
133 |
Ulnt |
Voltage phase imbalance trips count |
1 |
|
134 |
Ulnt |
Voltage phase loss trips count |
1 |
|
135 |
Ulnt |
Wiring trips count |
1 |
|
136 |
Ulnt |
Undervoltage trips count |
1 |
|
137 |
Ulnt |
Overvoltage trips count |
1 |
|
138 |
Ulnt |
Underpower trips count |
1 |
|
139 |
Ulnt |
Overpower trips count |
1 |
|
140 |
Ulnt |
Under power factor trips count |
1 |
|
141 |
Ulnt |
Over power factor trips count |
1 |
|
142 |
Ulnt |
Load sheddings count |
1 |
|
143-144 |
UDlnt |
Active power consumption (kWh) |
1 |
|
145-146 |
UDlnt |
Reactive power consumption (kVARh) |
1 |
|
147 |
Ulnt |
Auto restart immediate count |
|
|
148 |
Ulnt |
Auto restart delayed count |
|
|
149 |
Ulnt |
Auto restart manual count |
Last Trip (n-0) Statistics
The last trip statistics are completed by variables at addresses 300 to 310.
|
Register |
Variable Type |
Read-only Variables |
|
|---|---|---|---|
|
150 |
Ulnt |
Trip code n-0 |
|
|
151 |
Ulnt |
Motor full load current ratio n-0 (% FLC max) |
|
|
152 |
Ulnt |
Thermal capacity level n-0 (% trip level) |
|
|
153 |
Ulnt |
Average current ratio n-0 (% FLC) |
|
|
154 |
Ulnt |
L1 current ratio n-0 (% FLC) |
|
|
155 |
Ulnt |
L2 current ratio n-0 (% FLC) |
|
|
156 |
Ulnt |
L3 current ratio n-0 (% FLC) |
|
|
157 |
Ulnt |
Ground current ratio n-0 (x 0.1 % FLC min) |
|
|
158 |
Ulnt |
Full load current max n-0 (x 0.1 A) |
|
|
159 |
Ulnt |
Current phase imbalance n-0 (%) |
|
|
160 |
Ulnt |
Frequency n-0 (x 0.1 Hz) |
2 |
|
161 |
Ulnt |
Motor temperature sensor n-0 (x 0.1 Ω) |
|
|
162-165 |
Word[4] |
Date and time n-0 (See DT_DateTime) |
|
|
166 |
Ulnt |
Average voltage n-0 (V) |
1 |
|
167 |
Ulnt |
L3-L1 voltage n-0 (V) |
1 |
|
168 |
Ulnt |
L1-L2 voltage n-0 (V) |
1 |
|
169 |
Ulnt |
L2-L3 voltage n-0 (V) |
1 |
|
170 |
Ulnt |
Voltage phase imbalance n-0 (%) |
1 |
|
171 |
Ulnt |
Active power n-0 (x 0.1 kW) |
1 |
|
172 |
Ulnt |
Power factor n-0 (x 0.01) |
1 |
|
173-179 |
(Not significant) |
N-1 Trip Statistics
The n-1 trip statistics are completed by variables at addresses 330 to 340.
|
Register |
Variable Type |
Read-only Variables |
|
|---|---|---|---|
|
180 |
Ulnt |
Trip code n-1 |
|
|
181 |
Ulnt |
Motor full load current ratio n-1 (% FLC max) |
|
|
182 |
Ulnt |
Thermal capacity level n-1 (% trip level) |
|
|
183 |
Ulnt |
Average current ratio n-1 (% FLC) |
|
|
184 |
Ulnt |
L1 current ratio n-1 (% FLC) |
|
|
185 |
Ulnt |
L2 current ratio n-1 (% FLC) |
|
|
186 |
Ulnt |
L3 current ratio n-1 (% FLC) |
|
|
187 |
Ulnt |
Ground current ratio n-1 (x 0.1 % FLC min) |
|
|
188 |
Ulnt |
Full load current max n-1 (x 0.1 A) |
|
|
189 |
Ulnt |
Current phase imbalance n-1 (%) |
|
|
190 |
Ulnt |
Frequency n-1 (x 0.1 Hz) |
2 |
|
191 |
Ulnt |
Motor temperature sensor n-1 (x 0.1 Ω) |
|
|
192-195 |
Word[4] |
Date and time n-1 (See DT_DateTime) |
|
|
196 |
Ulnt |
Average voltage n-1 (V) |
1 |
|
197 |
Ulnt |
L3-L1 voltage n-1 (V) |
1 |
|
198 |
Ulnt |
L1-L2 voltage n-1 (V) |
1 |
|
199 |
Ulnt |
L2-L3 voltage n-1 (V) |
1 |
|
200 |
Ulnt |
Voltage phase imbalance n-1 (%) |
1 |
|
201 |
Ulnt |
Active power n-1 (x 0.1 kW) |
1 |
|
202 |
Ulnt |
Power factor n-1 (x 0.01) |
1 |
|
203-209 |
Ulnt |
(Not significant) |
N-2 Trip Statistics
The n-2 trip statistics are completed by variables at addresses 360 to 370.
|
Register |
Variable Type |
Read-only Variables |
|
|---|---|---|---|
|
210 |
Ulnt |
Trip code n-2 |
|
|
211 |
Ulnt |
Motor full load current ratio n-2 (% FLC max) |
|
|
212 |
Ulnt |
Thermal capacity level n-2 (% trip level) |
|
|
213 |
Ulnt |
Average current ratio n-2 (% FLC) |
|
|
214 |
Ulnt |
L1 current ratio n-2 (% FLC) |
|
|
215 |
Ulnt |
L2 current ratio n-2 (% FLC) |
|
|
216 |
Ulnt |
L3 current ratio n-2 (% FLC) |
|
|
217 |
Ulnt |
Ground current ratio n-2 (x 0.1 % FLC min) |
|
|
218 |
Ulnt |
Full load current max n-2 (x 0.1 A) |
|
|
219 |
Ulnt |
Current phase imbalance n-2 (%) |
|
|
220 |
Ulnt |
Frequency n-2 (x 0.1 Hz) |
2 |
|
221 |
Ulnt |
Motor temperature sensor n-2 (x 0.1 Ω) |
|
|
222-225 |
Word[4] |
Date and time n-2 (See DT_DateTime) |
|
|
226 |
Ulnt |
Average voltage n-2 (V) |
1 |
|
227 |
Ulnt |
L3-L1 voltage n-2 (V) |
1 |
|
228 |
Ulnt |
L1-L2 voltage n-2 (V) |
1 |
|
229 |
Ulnt |
L2-L3 voltage n-2 (V) |
1 |
|
230 |
Ulnt |
Voltage phase imbalance n-2 (%) |
1 |
|
231 |
Ulnt |
Active power n-2 (x 0.1 kW) |
1 |
|
232 |
Ulnt |
Power factor n-2 (x 0.01) |
1 |
|
233-239 |
(Not significant) |
N-3 Trip Statistics
The n-3 trip statistics are completed by variables at addresses 390 to 400.
|
Register |
Variable Type |
Read-only Variables |
|
|---|---|---|---|
|
240 |
Ulnt |
Trip code n-3 |
|
|
241 |
Ulnt |
Motor full load current ratio n-3 (% FLC max) |
|
|
242 |
Ulnt |
Thermal capacity level n-3 (% trip level) |
|
|
243 |
Ulnt |
Average current ratio n-3 (% FLC) |
|
|
244 |
Ulnt |
L1 current ratio n-3 (% FLC) |
|
|
245 |
Ulnt |
L2 current ratio n-3 (% FLC) |
|
|
246 |
Ulnt |
L3 current ratio n-3 (% FLC) |
|
|
247 |
Ulnt |
Ground current ratio n-3 (x 0.1 % FLC min) |
|
|
248 |
Ulnt |
Full load current max n-3 (0.1 A) |
|
|
249 |
Ulnt |
Current phase imbalance n-3 (%) |
|
|
250 |
Ulnt |
Frequency n-3 (x 0.1 Hz) |
2 |
|
251 |
Ulnt |
Motor temperature sensor n-3 (x 0.1 Ω) |
|
|
252-255 |
Word[4] |
Date and time n-3 (See DT_DateTime) |
|
|
256 |
Ulnt |
Average voltage n-3 (V) |
1 |
|
257 |
Ulnt |
L3-L1 voltage n-3 (V) |
1 |
|
258 |
Ulnt |
L1-L2 voltage n-3 (V) |
1 |
|
259 |
Ulnt |
L2-L3 voltage n-3 (V) |
1 |
|
260 |
Ulnt |
Voltage phase imbalance n-3 (%) |
1 |
|
261 |
Ulnt |
Active power n-3 (x 0.1 kW) |
1 |
|
262 |
Ulnt |
Power factor n-3 (x 0.01) |
1 |
|
263-269 |
(Not significant) |
N-4 Trip Statistics
The n-4 trip statistics are completed by variables at addresses 420 to 430.
|
Register |
Variable Type |
Read-only Variables |
|
|---|---|---|---|
|
270 |
Ulnt |
Trip code n-4 |
|
|
271 |
Ulnt |
Motor full load current ratio n-4 (% FLC max) |
|
|
272 |
Ulnt |
Thermal capacity level n-4 (% trip level) |
|
|
273 |
Ulnt |
Average current ratio n-4 (% FLC) |
|
|
274 |
Ulnt |
L1 current ratio n-4 (% FLC) |
|
|
275 |
Ulnt |
L2 current ratio n-4 (% FLC) |
|
|
276 |
Ulnt |
L3 current ratio n-4 (% FLC) |
|
|
277 |
Ulnt |
Ground current ratio n-4 (x 0.1 % FLC min) |
|
|
278 |
Ulnt |
Full load current max n-4 (x 0.1 A) |
|
|
279 |
Ulnt |
Current phase imbalance n-4 (%) |
|
|
280 |
Ulnt |
Frequency n-4 (x 0.1 Hz) |
2 |
|
281 |
Ulnt |
Motor temperature sensor n-4 (x 0.1 Ω) |
|
|
282-285 |
Word[4] |
Date and time n-4 (See DT_DateTime) |
|
|
286 |
Ulnt |
Average voltage n-4 (V) |
1 |
|
287 |
Ulnt |
L3-L1 voltage n-4 (V) |
1 |
|
288 |
Ulnt |
L1-L2 voltage n-4 (V) |
1 |
|
289 |
Ulnt |
L2-L3 voltage n-4 (V) |
1 |
|
290 |
Ulnt |
Voltage phase imbalance n-4 (%) |
1 |
|
291 |
Ulnt |
Active power n-4 (x 0.1 kW) |
1 |
|
292 |
Ulnt |
Power factor n-4 (x 0.01) |
1 |
|
293-299 |
(Not significant) |
Last Trip (n-0) Statistics Extension
The last trip main statistics are listed at addresses 150-179.
|
Register |
Variable Type |
Read-only Variables |
|
|---|---|---|---|
|
300-301 |
UDlnt |
Average current n-0 (x 0.01 A) |
|
|
302-303 |
UDlnt |
L1 current n-0 (x 0.01 A) |
|
|
304-305 |
UDlnt |
L2 current n-0 (x 0.01 A) |
|
|
306-307 |
UDlnt |
L3 current n-0 (x 0.01 A) |
|
|
308-309 |
UDlnt |
Ground current n-0 (mA) |
|
|
310 |
Ulnt |
Motor temperature sensor degree n-0 (°C) |
N-1 Trip Statistics Extension
The n-1 trip main statistics are listed at addresses 180-209.
|
Register |
Variable Type |
Read-only Variables |
|
|---|---|---|---|
|
330-331 |
UDlnt |
Average current n-1 (x 0.01 A) |
|
|
332-333 |
UDlnt |
L1 current n-1 (x 0.01 A) |
|
|
334-335 |
UDlnt |
L2 current n-1 (x 0.01 A) |
|
|
336-337 |
UDlnt |
L3 current n-1 (x 0.01 A) |
|
|
338-339 |
UDlnt |
Ground current n-1 (mA) |
|
|
340 |
Ulnt |
Motor temperature sensor degree n-1 (°C) |
N-2 Trip Statistics Extension
The n-2 trip main statistics are listed at addresses 210-239.
|
Register |
Variable Type |
Read-only Variables |
|
|---|---|---|---|
|
360-361 |
UDlnt |
Average current n-2 (x 0.01 A) |
|
|
362-363 |
UDlnt |
L1 current n-2 (x 0.01 A) |
|
|
364-365 |
UDlnt |
L2 current n-2 (x 0.01 A) |
|
|
366-367 |
UDlnt |
L3 current n-2 (x 0.01 A) |
|
|
368-369 |
UDlnt |
Ground current n-2 (mA) |
|
|
370 |
Ulnt |
Motor temperature sensor degree n-2 (°C) |
N-3 Trip Statistics Extension
The n-3 trip main statistics are listed at addresses 240-269.
|
Register |
Variable Type |
Read-only Variables |
|
|---|---|---|---|
|
390-391 |
UDlnt |
Average current n-3 (x 0.01 A) |
|
|
392-393 |
UDlnt |
L1 current n-3 (x 0.01 A) |
|
|
394-395 |
UDlnt |
L2 current n-3 (x 0.01 A) |
|
|
396-397 |
UDlnt |
L3 current n-3 (x 0.01 A) |
|
|
398-399 |
UDlnt |
Ground current n-3 (mA) |
|
|
400 |
Ulnt |
Motor temperature sensor degree n-3 (°C) |
N-4 Trip Statistics Extension
The n-4 trip main statistics are listed at addresses 270-299.
|
Register |
Variable Type |
Read-only Variables |
|
|---|---|---|---|
|
420-421 |
UDlnt |
Average current n-4 (x 0.01 A) |
|
|
422-423 |
UDlnt |
L1 current n-4 (x 0.01 A) |
|
|
424-425 |
UDlnt |
L2 current n-4 (x 0.01 A) |
|
|
426-427 |
UDlnt |
L3 current n-4 (x 0.01 A) |
|
|
428-429 |
UDlnt |
Ground current n-4 (mA) |
|
|
430 |
Ulnt |
Motor temperature sensor degree n-4 (°C) |
Monitoring Variables
Monitoring Overview
Monitoring variables are grouped according to the following criteria:
|
Monitoring Variable Groups |
Registers |
|---|---|
|
Monitoring of trips |
450 to 454 |
|
Monitoring of status |
455 to 459 |
|
Monitoring of alarms |
460 to 464 |
|
Monitoring of measurements |
465 to 539 |
Monitoring of Trips
Variables for monitoring of trips are described in the following table:
|
Register |
Variable Type |
Read-only Variables |
|
|---|---|---|---|
|
450 |
Ulnt |
Minimum wait time (s) |
|
|
451 |
Ulnt |
Trip code (code of the last trip, or of the trip that takes priority) (See DT_TripCode.) |
|
|
452 |
Word |
Trip register 1 |
|
|
bits 0-1 (Reserved) |
|||
|
bit 2 Ground current trip |
|||
|
bit 3 Thermal overload trip |
|||
|
bit 4 Long start trip |
|||
|
bit 5 Jam trip |
|||
|
bit 6 Current phase imbalance trip |
|||
|
bit 7 Undercurrent trip |
|||
|
bit 8 (Reserved) |
|||
|
bit 9 Test trip |
|||
|
bit 10 HMI port trip |
|||
|
bit 11 Controller internal trip |
|||
|
bit 12 Internal port trip |
|||
|
bit 13 (Not significant) |
|||
|
bit 14 Network port config trip |
|||
|
bit 15 Network port trip |
|||
|
453 |
Word |
Trip register 2 |
|
|
bit 0 External system trip |
|||
|
bit 1 Diagnostic trip |
|||
|
bit 2 Wiring trip |
|||
|
bit 3 Overcurrent trip |
|||
|
bit 4 Current phase loss trip |
|||
|
bit 5 Current phase reversal trip |
|||
|
bit 6 Motor temperature sensor trip |
1 |
||
|
bit 7 Voltage phase imbalance trip |
1 |
||
|
bit 8 Voltage phase loss trip |
1 |
||
|
bit 9 Voltage phase reversal trip |
1 |
||
|
bit 10 Undervoltage trip |
1 |
||
|
bit 11 Overvoltage trip |
1 |
||
|
bit 12 Underpower trip |
1 |
||
|
bit 13 Overpower trip |
1 |
||
|
bit 14 Under power factor trip |
1 |
||
|
bit 15 Over power factor trip |
1 |
||
|
454 |
Word |
Trip register 3 |
|
|
bit 0 LTME configuration trip |
|||
|
bit 1 LTMR configuration trip |
|||
|
bits 2-15 (Reserved) |
Monitoring of Status
Variables for monitoring of status are described in the following table:
|
Register |
Variable Type |
Read-only Variables |
|
|---|---|---|---|
|
455 |
Word |
System status register 1 |
|
|
bit 0 System ready |
|||
|
bit 1 System on |
|||
|
bit 2 System trip |
|||
|
bit 3 System alarm |
|||
|
bit 4 System tripped |
|||
|
bit 5 Trip reset authorized |
|||
|
bit 6 Controller power |
|||
|
bit 7 Motor running (with detection of a current, if greater than 10% FLC) |
|||
|
bits 8-13 Motor average current ratio 32 = 100% FLC - 63 = 200% FLC |
|||
|
bit 14 In remote |
|||
|
bit 15 Motor starting (start in progress) 0 = descending current is less than 150% FLC 1 = ascending current is greater than 10% FLC |
|||
|
456 |
Word |
System status register 2 |
|
|
bit 0 Auto-reset active |
|||
|
bit 1 (Not significant) |
|||
|
bit 2 Trip power cycle requested |
|||
|
bit 3 Motor restart time undefined |
|||
|
bit 4 Rapid cycle lockout |
|||
|
bit 5 Load shedding |
1 |
||
|
bit 6 Motor speed 0 = FLC1 setting is used 1 = FLC2 setting is used |
|||
|
bit 7 HMI port comm loss |
|||
|
bit 8 Network port comm loss |
|||
|
bit 9 Motor transition lockout |
|||
|
bits 10-15 (Not significant) |
|||
|
457 |
Word |
Logic inputs status |
|
|
bit 0 Logic input 1 |
|||
|
bit 1 Logic input 2 |
|||
|
bit 2 Logic input 3 |
|||
|
bit 3 Logic input 4 |
|||
|
bit 4 Logic input 5 |
|||
|
bit 5 Logic input 6 |
|||
|
bit 6 Logic input 7 |
1 |
||
|
bit 7 Logic input 8 |
1 |
||
|
bit 8 Logic input 9 |
1 |
||
|
bit 9 Logic input 10 |
1 |
||
|
bit 10 Logic input 11 |
1 |
||
|
bit 11 Logic input 12 |
1 |
||
|
bit 12 Logic input 13 |
1 |
||
|
bit 13 Logic input 14 |
1 |
||
|
bit 14 Logic input 15 |
1 |
||
|
bit 15 Logic input 16 |
1 |
||
|
458 |
Word |
Logic outputs status |
|
|
bit 0 Logic output 1 |
|||
|
bit 1 Logic output 2 |
|||
|
bit 2 Logic output 3 |
|||
|
bit 3 Logic output 4 |
|||
|
bit 4 Logic output 5 |
1 |
||
|
bit 5 Logic output 6 |
1 |
||
|
bit 6 Logic output 7 |
1 |
||
|
bit 7 Logic output 8 |
1 |
||
|
bits 8-15 (Reserved) |
|||
|
459 |
Word |
I/O status |
|
|
bit 0 Input 1 |
|||
|
bit 1 Input 2 |
|||
|
bit 2 Input 3 |
|||
|
bit 3 Input 4 |
|||
|
bit 4 Input 5 |
|||
|
bit 5 Input 6 |
|||
|
bit 6 Input 7 |
|||
|
bit 7 Input 8 |
|||
|
bit 8 Input 9 |
|||
|
bit 9 Input 10 |
|||
|
bit 10 Input 11 |
|||
|
bit 11 Input 12 |
|||
|
bit 12 Output 1 (13-14) |
|||
|
bit 13 Output 2 (23-24) |
|||
|
bit 14 Output 3 (33-34) |
|||
|
bit 15 Output 4 (95-96, 97-98) |
Monitoring of Alarms
Variables for monitoring of alarms are described in the following table:
|
Register |
Variable Type |
Read-only Variables |
|
|---|---|---|---|
|
460 |
UInt |
Alarm code (See DT_AlarmCode.) |
|
|
461 |
Word |
Alarm register 1 |
|
|
bits 0-1 (Not significant) |
|||
|
bit 2 Ground current alarm |
|||
|
bit 3 Thermal overload alarm |
|||
|
bit 4 (Not significant) |
|||
|
bit 5 Jam alarm |
|||
|
bit 6 Current phase imbalance alarm |
|||
|
bit 7 Undercurrent alarm |
|||
|
bits 8-9 (Not significant) |
|||
|
bit 10 HMI port alarm |
|||
|
bit 11 Controller internal temperature alarm |
|||
|
bits 12-14 (Not significant) |
|||
|
bit 15 Network port alarm |
|||
|
462 |
Word |
Alarm register 2 |
|
|
bit 0 (Not significant) |
|||
|
bit 1 Diagnostic alarm |
|||
|
bit 2 (Reserved) |
|||
|
bit 3 Overcurrent alarm |
|||
|
bit 4 Current phase loss alarm |
|||
|
bit 5 Current phase reversal alarm |
|||
|
bit 6 Motor temperature sensor alarm |
|||
|
bit 7 Voltage phase imbalance alarm |
1 |
||
|
bit 8 Voltage phase loss alarm |
1 |
||
|
bit 9 (Not significant) |
1 |
||
|
bit 10 Undervoltage alarm |
1 |
||
|
bit 11 Overvoltage alarm |
1 |
||
|
bit 12 Underpower alarm |
1 |
||
|
bit 13 Overpower alarm |
1 |
||
|
bit 14 Under power factor alarm |
1 |
||
|
bit 15 Over power factor alarm |
1 |
||
|
463 |
Word |
Alarm register 3 |
|
|
bit 0 LTME configuration alarm |
|||
|
bits 1-15 (Reserved) |
|||
|
464 |
UInt |
Motor temperature sensor degree (°C) |
Monitoring of Measurements
Variables for monitoring of measurements are described in the following table:
|
Register |
Variable Type |
Read-only Variables |
|
|---|---|---|---|
|
465 |
UInt |
Thermal capacity level (% trip level) |
|
|
466 |
UInt |
Average current ratio (% FLC) |
|
|
467 |
UInt |
L1 current ratio (% FLC) |
|
|
468 |
UInt |
L2 current ratio (% FLC) |
|
|
469 |
UInt |
L3 current ratio (% FLC) |
|
|
470 |
UInt |
Ground current ratio (x 0.1 % FLC min) |
|
|
471 |
UInt |
Current phase imbalance (%) |
|
|
472 |
Int |
Controller internal temperature (°C) |
|
|
473 |
UInt |
Controller config checksum |
|
|
474 |
UInt |
Frequency (x 0.01 Hz) |
2 |
|
475 |
UInt |
Motor temperature sensor (x 0.1 Ω) |
|
|
476 |
UInt |
Average voltage (V) |
1 |
|
477 |
UInt |
L3-L1 voltage (V) |
1 |
|
478 |
UInt |
L1-L2 voltage (V) |
1 |
|
479 |
UInt |
L2-L3 voltage (V) |
1 |
|
480 |
UInt |
Voltage phase imbalance (%) |
1 |
|
481 |
UInt |
Power factor (x 0.01) |
1 |
|
482 |
UInt |
Active power (x 0.1 kW) |
1 |
|
483 |
UInt |
Reactive power (x 0.1 kVAR) |
1 |
|
484 |
Word |
Auto restart status register |
|
|
bit 0 Voltage dip occurred |
|||
|
bit 1 Voltage dip detection |
|||
|
bit 2 Auto restart immediate condition |
|||
|
bit 3 Auto restart delayed condition |
|||
|
bit 4 Auto restart manual condition |
|||
|
bits 5-15 (Not significant) |
|||
|
485 |
Word |
Controller last power off duration |
|
|
486-489 |
Word |
(Not significant) |
|
|
490 |
Word |
Network port monitoring |
|
|
bit 0 Network port monitoring |
|||
|
bit 1 Network port connected |
|||
|
bit 2 Network port self-testing |
|||
|
bit 3 Network port self-detecting |
|||
|
bit 4 Network port bad config |
|||
|
bits 5-15 (Not significant) |
|||
|
491 |
UInt |
Network port baud rate (See DT_ExtBaudRate.) |
|
|
492 |
(Not significant) |
||
|
493 |
UInt |
Network port parity (See DT_ExtParity.) |
|
|
494-499 |
|
(Not significant) |
|
|
500-501 |
UDInt |
Average current (x 0.01 A) |
|
|
502-503 |
UDInt |
L1 current (x 0.01 A) |
|
|
504-505 |
UDInt |
L2 current (x 0.01 A) |
|
|
506-507 |
UDInt |
L3 current (x 0.01 A) |
|
|
508-509 |
UDInt |
Ground current (mA) |
|
|
510 |
UInt |
Controller port ID |
|
|
511 |
UInt |
Time to trip (x 1 s) |
|
|
512 |
UInt |
Motor last start current ratio (% FLC) |
|
|
513 |
UInt |
Motor last start duration (s) |
|
|
514 |
UInt |
Motor starts per hour count |
|
|
515 |
Word |
Phase imbalances register |
|
|
bit 0 L1 current highest imbalance |
|||
|
bit 1 L2 current highest imbalance |
|||
|
bit 2 L3 current highest imbalance |
|||
|
bit 3 L1-L2 voltage highest imbalance |
1 |
||
|
bit 4 L2-L3 voltage highest imbalance |
1 |
||
|
bit 5 L3-L1 voltage highest imbalance |
1 |
||
|
bits 6-15 (Not significant) |
|||
|
516 - 523 |
(Reserved) |
||
|
524 - 539 |
(Forbidden) |
Configuration Variables
Configuration Overview
Configuration variables are grouped according to the following criteria:
|
Configuration Variable Groups |
Registers |
|---|---|
|
Configuration |
540 to 649 |
|
Setting |
650 to 699 |
Configuration Variables
The configuration variables are described in the following table:
|
Register |
Variable Type |
Read / Write Variables |
|
|---|---|---|---|
|
540 |
UInt |
Motor operating mode 2 = 2-wire overload 3 = 3-wire overload 4 = 2-wire independent 5 = 3-wire independent 6 = 2-wire reverser 7 = 3-wire reverser 8 = 2-wire 2-step 9 = 3-wire 2-step 10 = 2-wire 2-speed 11 = 3-wire 2-speed 256-511 = Custom logic program (0-255) |
B |
|
541 |
UInt |
Motor transition timeout (s) |
|
|
542-544 |
(Reserved) |
||
|
545 |
Word |
Controller AC inputs setting register |
|
|
bits 0-3 Controller AC logic inputs configuration (see DC_ACInputSetting) |
|||
|
bits 4-15 (Reserved) |
|||
|
546 |
UInt |
Thermal overload setting |
B |
|
bits 0-2 Motor temperature sensor type 0 = None 1 = PTC binary 2 = PT100 3 = PTC analog 4 = NTC analog |
|||
|
bits 3-4 Thermal overload mode 0 = Definite 2 = Inverse thermal |
|||
|
bits 5-15 (Reserved) |
|||
|
547 |
UInt |
Thermal overload trip definite timeout (s) |
|
|
548 |
(Reserved) |
||
|
549 |
UInt |
Motor temperature sensor trip threshold (x 0.1 Ω) |
|
|
550 |
UInt |
Motor temperature sensor alarm threshold (x 0.1 Ω) |
|
|
551 |
UInt |
Motor temperature sensor trip threshold degree (°C) |
|
|
552 |
UInt |
Motor temperature sensor alarm threshold degree (°C) |
|
|
553 |
UInt |
Rapid cycle lockout timeout (s) |
|
|
554 |
(Reserved) |
||
|
555 |
UInt |
Current phase loss timeout (x 0.1 s) |
|
|
556 |
UInt |
Overcurrent trip timeout (s) |
|
|
557 |
UInt |
Overcurrent trip threshold (% FLC) |
|
|
558 |
UInt |
Overcurrent alarm threshold (% FLC) |
|
|
559 |
Word |
Ground current trip configuration |
B |
|
bit 0 Ground current mode |
|||
|
bit 1 Ground trip disabled while starting |
|||
|
bits 2-15 (Reserved) |
|||
|
560 |
UInt |
Ground current sensor primary |
|
|
561 |
UInt |
Ground current sensor secondary |
|
|
562 |
UInt |
External ground current trip timeout (x 0.01 s) |
|
|
563 |
UInt |
External ground current trip threshold (x 0.01 A) |
|
|
564 |
UInt |
External ground current alarm threshold (x 0.01 A) |
|
|
565 |
UInt |
Motor nominal voltage (V) |
1 |
|
566 |
UInt |
Voltage phase imbalance trip timeout starting (x 0.1 s) |
1 |
|
567 |
UInt |
Voltage phase imbalance trip timeout running (x 0.1 s) |
1 |
|
568 |
UInt |
Voltage phase imbalance trip threshold (% imb) |
1 |
|
569 |
UInt |
Voltage phase imbalance alarm threshold (% imb) |
1 |
|
570 |
UInt |
Overvoltage trip timeout (x 0.1 s) |
1 |
|
571 |
UInt |
Overvoltage trip threshold (% Vnom) |
1 |
|
572 |
UInt |
Overvoltage alarm threshold (% Vnom) |
1 |
|
573 |
UInt |
Undervoltage trip timeout |
1 |
|
574 |
UInt |
Undervoltage trip threshold (% Vnom) |
1 |
|
575 |
UInt |
Undervoltage alarm threshold (% Vnom) |
1 |
|
576 |
UInt |
Voltage phase loss trip timeout (x 0.1 s) |
1 |
|
577 |
Word |
Voltage dip setting |
1 |
|
bits 0-1 Voltage dip mode 0 = None (factory setting) 1 = Load shedding 2 = Auto-restart |
|||
|
bits 3-15 (Reserved) |
|||
|
578 |
UInt |
Load shedding timeout (s) |
1 |
|
579 |
UInt |
Voltage dip threshold (% Vnom) |
1 |
|
580 |
UInt |
Voltage dip restart timeout (s) |
1 |
|
581 |
UInt |
Voltage dip restart threshold (% Vnom) |
1 |
|
582 |
UInt |
Auto restart immediate timeout (x 0.1 s) |
|
|
583 |
UInt |
Motor nominal power (x 0.1 kW) |
1 |
|
584 |
UInt |
Overpower trip timeout (s) |
1 |
|
585 |
UInt |
Overpower trip threshold (% Pnom) |
1 |
|
586 |
UInt |
Overpower alarm threshold (% Pnom) |
1 |
|
587 |
UInt |
Underpower trip timeout (s) |
1 |
|
588 |
UInt |
Underpower trip threshold (% Pnom) |
1 |
|
589 |
UInt |
Underpower alarm threshold (% Pnom) |
1 |
|
590 |
UInt |
Under power factor trip timeout (x 0.1 s) |
1 |
|
591 |
UInt |
Under power factor trip threshold (x 0.01 PF) |
1 |
|
592 |
UInt |
Under power factor alarm threshold (x 0.01 PF) |
1 |
|
593 |
UInt |
Over power factor trip timeout (x 0.1 s) |
1 |
|
594 |
UInt |
Over power factor trip threshold (x 0.01 PF) |
1 |
|
595 |
UInt |
Over power factor alarm threshold (x 0.01 PF) |
1 |
|
596 |
UInt |
Auto restart delayed timeout (s) |
|
|
597-599 |
(Reserved) |
||
|
600 |
(Not significant) |
||
|
601 |
Word |
General configuration register 1 |
|
|
bit 0 Controller system config required 0 = exit the configuration menu 1 = go to the configuration menu |
A |
||
|
bits 1-7 (Reserved) |
|||
|
Control mode configuration, bits 8-10 (one bit is set to 1): |
|||
|
bit 8 Config via HMI keypad enable |
|||
|
bit 9 Config via HMI engineering tool enable |
|||
|
bit 10 Config via network port enable |
|||
|
bit 11 Motor star-delta |
B |
||
|
bit 12 Motor phases sequence 0 = A B C 1 = A C B |
|||
|
bits 13-14 Motor phases (see DT_PhaseNumber) |
B |
||
|
bit 15 Motor auxiliary fan cooled (factory setting = 0) |
|||
|
602 |
Word |
General configuration register 2 |
|
|
bits 0-2 Trip reset mode (see DT_ResetMode) |
C |
||
|
bit 3 HMI port parity setting 0 = none 1 = even (factory setting) |
|||
|
bits 4-8 (Reserved) |
|||
|
bit 9 HMI port endian setting |
|||
|
bit 10 Network port endian setting |
|||
|
bit 11 HMI motor status LED color |
|||
|
bits 12-15 (Reserved) |
|||
|
603 |
Ulnt |
HMI port address setting |
|
|
604 |
Ulnt |
HMI port baud rate setting (Baud) |
|
|
605 |
(Reserved) |
||
|
606 |
Ulnt |
Motor trip class (s) |
|
|
607 |
(Reserved) |
||
|
608 |
Ulnt |
Thermal overload trip reset threshold (% trip level) |
|
|
609 |
Ulnt |
Thermal overload alarm threshold (% trip level) |
|
|
610 |
UInt |
Internal ground current trip timeout (x 0.1 s) |
|
|
611 |
UInt |
Internal ground current trip threshold (% FLCmin) |
|
|
612 |
UInt |
Internal ground current alarm threshold (% FLCmin) |
|
|
613 |
UInt |
Current phase imbalance trip timeout starting (x 0.1 s) |
|
|
614 |
UInt |
Current phase imbalance trip timeout running (x 0.1 s) |
|
|
615 |
UInt |
Current phase imbalance trip threshold (% imb) |
|
|
616 |
UInt |
Current phase imbalance alarm threshold (% imb) |
|
|
617 |
UInt |
Jam trip timeout (s) |
|
|
618 |
UInt |
Jam trip threshold (% FLC) |
|
|
619 |
UInt |
Jam alarm threshold (% FLC) |
|
|
620 |
UInt |
Undercurrent trip timeout (s) |
|
|
621 |
UInt |
Undercurrent trip threshold (% FLC) |
|
|
622 |
UInt |
Undercurrent alarm threshold (% FLC) |
|
|
623 |
UInt |
Long start trip timeout (s) |
|
|
624 |
UInt |
Long start trip threshold (% FLC) |
|
|
625 |
(Reserved) |
||
|
626 |
UInt |
HMI display contrast setting |
|
|
bits 0-7 HMI display contrast setting |
|||
|
bits 8-15 HMI display brightness setting |
|||
|
627 |
UInt |
Contactor rating (0.1 A) |
|
|
628 |
UInt |
Load CT primary |
B |
|
629 |
UInt |
Load CT secondary |
B |
|
630 |
UInt |
Load CT multiple passes (passes) |
B |
|
631 |
Word |
Trip enable register 1 |
|
|
bits 0-1 (Reserved) |
|||
|
bit 2 Ground current trip enable |
|||
|
bit 3 Thermal overload trip enable |
|||
|
bit 4 Long start trip enable |
|||
|
bit 5 Jam trip enable |
|||
|
bit 6 Current phase imbalance trip enable |
|||
|
bit 7 Undercurrent trip enable |
|||
|
bit 8 (Reserved) |
|||
|
bit 9 Self test enable 0 = disable 1 = enable (factory setting) |
|||
|
bit 10 HMI port trip enable |
|||
|
bits 11-14 (Reserved) |
|||
|
bit 15 Network port trip enable |
|||
|
632 |
Word |
Alarm enable register 1 |
|
|
bit 0 (Not significant) |
|||
|
bit 1 (Reserved) |
|||
|
bit 2 Ground current alarm enable |
|||
|
bit 3 Thermal overload alarm enable |
|||
|
bit 4 (Reserved) |
|||
|
bit 5 Jam alarm enable |
|||
|
bit 6 Current phase imbalance alarm enable |
|||
|
bit 7 Undercurrent alarm enable |
|||
|
bits 8- 9 (Reserved) |
|||
|
bit 10 HMI port alarm enable |
|||
|
bit 11 Controller internal temperature alarm enable |
|||
|
bits 12-14 (Reserved) |
|||
|
bit 15 Network port alarm enable |
|||
|
633 |
Word |
Trip enable register 2 |
|
|
bit 0 (Reserved) |
|||
|
bit 1 Diagnostic trip enable |
|||
|
bit 2 Wiring trip enable |
|||
|
bit 3 Overcurrent trip enable |
|||
|
bit 4 Current phase loss trip enable |
|||
|
bit 5 Current phase reversal trip enable |
|||
|
bit 6 Motor temperature sensor trip enable |
|||
|
bit 7 Voltage phase imbalance trip enable |
1 |
||
|
bit 8 Voltage phase loss trip enable |
1 |
||
|
bit 9 Voltage phase reversal trip enable |
1 |
||
|
bit 10 Undervoltage trip enable |
1 |
||
|
bit 11 Overvoltage trip enable |
1 |
||
|
bit 12 Underpower trip enable |
1 |
||
|
bit 13 Overpower trip enable |
1 |
||
|
bit 14 Under power factor trip enable |
1 |
||
|
bit 15 Over power factor trip enable |
1 |
||
|
634 |
Word |
Alarm enable register 2 |
|
|
bit 0 (Reserved) |
|||
|
bit 1 Diagnostic alarm enable |
|||
|
bit 2 (Reserved) |
|||
|
bit 3 Overcurrent alarm enable |
|||
|
bit 4 Current phase loss alarm enable |
|||
|
bit 5 (Reserved) |
|||
|
bit 6 Motor temperature sensor alarm enable |
|||
|
bit 7 Voltage phase imbalance alarm enable |
1 |
||
|
bit 8 Voltage phase loss alarm enable |
1 |
||
|
bit 9 (Reserved) |
1 |
||
|
bit 10 Undervoltage alarm enable |
1 |
||
|
bit 11 Overvoltage alarm enable |
1 |
||
|
bit 12 Underpower alarm enable |
1 |
||
|
bit 13 Overpower alarm enable |
1 |
||
|
bit 14 Under power factor alarm enable |
1 |
||
|
bit 15 Over power factor alarm enable |
1 |
||
|
635-6 |
(Reserved) |
||
|
637 |
UInt |
Auto-reset attempts group 1 setting (resets) |
|
|
638 |
UInt |
Auto-reset group 1 timeout (s) |
|
|
639 |
UInt |
Auto-reset attempts group 2 setting (resets) |
|
|
640 |
UInt |
Auto-reset group 2 timeout (s) |
|
|
641 |
UInt |
Auto-reset attempts group 3 setting (resets) |
|
|
642 |
UInt |
Auto-reset group 3 timeout (s) |
|
|
643 |
UInt |
Motor step 1 to 2 timeout (x 0.1 s) |
|
|
644 |
UInt |
Motor step 1 to 2 threshold (% FLC) |
|
|
645 |
UInt |
HMI port fallback setting |
|
|
646-649 |
(Reserved) |
Setting Variables
The setting variables are described in the following table:
|
Register |
Variable Type |
Read / Write Variables |
|
|---|---|---|---|
|
650 |
Word |
HMI language setting register: |
|
|
bits 0-4 HMI language setting (see DT_Language5) |
|||
|
bits 5-15 (Not significant) |
|||
|
651 |
Word |
HMI display items register 1 |
|
|
bit 0 HMI display average current enable |
|||
|
bit 1 HMI display thermal capacity level enable |
|||
|
bit 2 HMI display L1 current enable |
|||
|
bit 3 HMI display L2 current enable |
|||
|
bit 4 HMI display L3 current enable |
|||
|
bit 5 HMI display ground current enable |
|||
|
bit 6 HMI display motor status enable |
|||
|
bit 7 HMI display current phase imbalance enable |
|||
|
bit 8 HMI display operating time enable |
|||
|
bit 9 HMI display I/O status enable |
|||
|
bit 10 HMI display reactive power enable |
|||
|
bit 11 HMI display frequency enable |
|||
|
bit 12 HMI display starts per hour enable |
|||
|
bit 13 HMI display control mode enable |
|||
|
bit 14 HMI display start statistics enable |
|||
|
bit 15 HMI motor temperature sensor enable |
|||
|
652 |
Ulnt |
Motor full load current ratio, FLC1 (% FLCmax) |
|
|
653 |
Ulnt |
Motor high speed full load current ratio, FLC2 (% FLCmax) |
|
|
654 |
Word |
HMI display items register 2 |
|
|
bit 0 HMI display L1-L2 voltage enable |
1 |
||
|
bit 1 HMI display L2-L3 voltage enable |
1 |
||
|
bit 2 HMI display L3-L1 voltage enable |
1 |
||
|
bit 3 HMI display average voltage enable |
1 |
||
|
bit 4 HMI display active power enable |
1 |
||
|
bit 5 HMI display power consumption enable |
1 |
||
|
bit 6 HMI display power factor enable |
1 |
||
|
bit 7 HMI display average current ratio enable |
|||
|
bit 8 HMI display L1 current ratio enable |
1 |
||
|
bit 9 HMI display L2 current ratio enable |
1 |
||
|
bit 10 HMI display L3 current ratio enable |
1 |
||
|
bit 11 HMI display thermal capacity remaining enable |
|||
|
bit 12 HMI display time to trip enable |
|||
|
bit 13 HMI display voltage phase imbalance enable |
1 |
||
|
bit 14 HMI display date enable |
|||
|
bit 15 HMI display time enable |
|||
|
655-658 |
Word[4] |
Date and time setting (See DT_DateTime) |
|
|
659 |
Word |
HMI display items register 3 |
|
|
bit 0 HMI display temperature sensor degree CF |
|||
|
bits 1-15 (Reserved) |
|||
|
660-681 |
(Reserved) |
||
|
682 |
Ulnt |
Network port fallback setting (see DT_OutputFallbackStrategy) |
|
|
683 |
Word |
Control setting register |
|
|
bits 0-1 (Reserved) |
|||
|
bit 2 Control remote local default mode (with LTMCU) 0 = remote 1 = local |
|||
|
bit 3 (Reserved) |
|||
|
bit 4 Control remote local buttons enable (with LTMCU) 0 = disable 1 = enable |
|||
|
bits 5-6 Control remote channel setting (with LTMCU) 0 = network 1 = terminal strip 2 = HMI |
|||
|
bit 7 (Reserved) |
|||
|
bit 8 Control local channel setting 0 = terminal strip 1 = HMI |
|||
|
bit 9 Control direct transition 0 = stop required during transition 1 = stop not required during transition |
|||
|
bit 10 Control transfer mode 0 = bump 1 = bumpless |
|||
|
bit 11 Stop terminal strip disable 0 = enable 1 = disable |
|||
|
bit 12 Stop HMI disable 0 = enable 1 = disable |
|||
|
bits 13-15 (Reserved) |
|||
|
684-692 |
(Reserved) |
||
|
693 |
Ulnt |
Network port comm loss timeout (x 0.01 s) (Modbus only) |
|
|
694 |
Ulnt |
Network port parity setting (Modbus only) |
|
|
695 |
Ulnt |
Network port baud rate setting (Baud) (see DT_ExtBaudRate) |
|
|
696 |
Ulnt |
Network port address setting |
|
|
697-699 |
(Not significant) |
Command Variables
Command Variables
Command variables are described in the following table:
|
Register |
Variable Type |
Read / Write Variables |
|
|---|---|---|---|
|
700 |
Word |
Register available to remotely write commands that can be processed in a specific custom logic |
|
|
701-703 |
(Reserved) |
||
|
704 |
Word |
Control register 1 |
|
|
bit 0 Motor run forward command * |
|||
|
bit 1 Motor run reverse command * |
|||
|
bit 2 (Reserved) |
|||
|
bit 3 Trip reset command |
|||
|
bit 4 (Reserved) |
|||
|
bit 5 Self test command |
|||
|
bit 6 Motor low speed command |
|||
|
bits 7-15 (Reserved) |
|||
|
705 |
Word |
Control register 2 |
|
|
bit 0 Clear all command Clear all parameters, except:
|
|||
|
bit 1 Clear statistics command |
|||
|
bit 2 Clear thermal capacity level command |
|||
|
bit 3 Clear controller settings command |
|||
|
bit 4 Clear network port settings command |
|||
|
bits 5-15 (Reserved) |
|||
|
706-709 |
(Reserved) |
||
|
710-799 |
(Forbidden) |
User Map Variables
Custom Logic Variables
Custom Logic Variables
Custom logic variables are described in the following table:
|
Register |
Variable Type |
Read-only Variables |
|
|---|---|---|---|
|
1200 |
Word |
Custom logic status register |
|
|
bit 0 Custom logic run |
|||
|
bit 1 Custom logic stop |
|||
|
bit 2 Custom logic reset |
|||
|
bit 3 Custom logic second step |
|||
|
bit 4 Custom logic transition |
|||
|
bit 5 Custom logic phase reverse |
|||
|
bit 6 Custom logic network control |
|||
|
bit 7 Custom logic FLC selection |
|||
|
bit 8 (Reserved) |
|||
|
bit 9 Custom logic auxiliary 1 LED |
|||
|
bit 10 Custom logic auxiliary 2 LED |
|||
|
bit 11 Custom logic stop LED |
|||
|
bit 12 Custom logic LO1 |
|||
|
bit 13 Custom logic LO2 |
|||
|
bit 14 Custom logic LO3 |
|||
|
bit 15 Custom logic LO4 |
|||
|
1201 |
Word |
Custom logic version |
|
|
1202 |
Word |
Custom logic memory space |
|
|
1203 |
Word |
Custom logic memory used |
|
|
1204 |
Word |
Custom logic temporary space |
|
|
1205 |
Word |
Custom logic non volatile space |
|
|
1206-1249 |
(Reserved) |
|
Register |
Variable Type |
Read/Write Variables |
|
|---|---|---|---|
|
1250 |
Word |
Custom logic setting register 1 |
|
|
bit 0 (Reserved) |
|||
|
bit 1 Logic input 3 external ready enable |
|||
|
bits 2-15 (Reserved) |
|||
|
1251-1269 |
(Reserved) |
||
|
1270 |
Word |
Custom logic command register 1 |
|
|
bit 0 Custom logic external trip command |
|||
|
bits 1-15 (Reserved) |
|||
|
1271-1279 |
(Reserved) |
|
Register |
Variable Type |
Read-only Variables |
|
|---|---|---|---|
|
1280 |
Word |
Custom logic monitoring register 1 |
|
|
bit 0 (Reserved) |
|||
|
bit 1 Custom logic system ready |
|||
|
bits 2-15 (Reserved) |
|||
|
1281-1300 |
(Reserved) |
|
Register |
Variable Type |
Read/Write Variables |
|
|---|---|---|---|
|
1301-1399 |
Word[99] |
General purpose registers for logic functions |
WARNING