DOCA0279EN-00

Installation

Installation Preparation

Administrator or equivalent privilege is required to install the TeSys Tera DTM Library on PC.

Installation Language

The language of the Installation dialog box is derived from the user language setting pre-defined by the operating system.

If the user language does not match any of the languages supported by the installation, the Installation dialog box will be displayed in english by default.

For more information about Installation of TeSys Tera DTM Library, refer to TeSys Tera Motor Management System DTM Library Online Help Guide – DOCA0275EN.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?