DOCA0279EN-00

TeSys Tera DTM Library Versions

The following versions of the TeSys Tera DTM Library are applicable for:

  • LTMT main unit with Modbus RTU communication protocol

  • LTMT main unit with PROFIBUS DP communication protocol

Version

Release

TeSys Tera DTM Library v2.0.0

Serial global release

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?