DOCA0279EN-00

FAQ

  • TeSys Tera DTM Library not appearing in the Catalog window:

    TeSys Tera DTM Library does not appear in the Catalog window in SoMove software after the DTM installation.

    Workaround: Follow the below steps to register the .dll file required for TeSys Tera DTM Library:

    1. Launch the Command Prompt window as administrator and enter the following command:

      cd C:\Windows\Microsoft.NET\Framework\v2.0.50727

    2. Enter the following command:

      RegAsm.exe /codebase “C:\Program Files (x86)\Common Files\Schneider Electric Shared\Schneider Electric TeSys Tera DTM Library\TeSysTerraDtm.Kernel.dll”

      Result: When the registration is successful, a pop-up message will be displayed.

    3. Launch the SoMove software. The Catalog Update screen with progress bar will appear.

      Result: After the catalog update is completed, the TeSys Tera DTM Library will be available in the Catalog window.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?