DOCA0276EN-02

Compatibility

The following table shows the compatibility of configuration or programming softwares with the TeSys Tera system in active releases.

TeSys Tera firmware package version

DTM version

LTMTCUF control operator unit firmware version

LTMTCUF Programmer tool version

TeSysTera_Ethernet_V001.000.004.sedp (LTMTE••)

DTM v2.0.1

TeSys Tera_HMI_V002.000.027_sedp

Integrated to DTM

TeSysTera_Ethernet_V001.000.003.sedp (LTMTE••)

DTM v2.0.1

TeSys Tera_HMI_V002.000.027_sedp

Integrated to DTM

TeSysTera_Ethernet_V001.000.000.sedp (LTMTE••)

DTM v2.0.1

TeSys Tera_HMI_V002.000.026_sedp

Integrated to DTM

TeSysTera_Serial_V002.001.002.sedp (LTMTM•• and LTMTP••)

DTM v2.0.1

TeSys Tera_HMI_V002.000.027_sedp

Integrated to DTM

TeSysTera_Serial_V002.000.000.sedp (LTMTM•• and LTMTP••)

DTM v2.0.1

TeSys Tera_HMI_V002.000.027_sedp

Integrated to DTM

NOTE: For TeSys Tera Ethernet, if firmware version is less than TeSys Tera_Ethernet_V001.000.003.sedp, then it requires a mandatory update to version TeSys Tera_Ethernet_V001.000.003.sedp
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.