DOCA0356EN-01

Clearance Zone Dimensions

For Electromagnetic Compatibility (EMC), it is recommended to mount a contactor at a distance of more than 100 mm (3.93 in) from the LTMT main unit and LTMT expansion module.

The clearance dimension of contactor from LTMT main unit and LTMT expansion module are shown below:

For more information on clearance dimension, refer to the Okken and BlokSeT Communications Cabling and Wiring Guide (available on request).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?