DOCA0356EN-01

Unboxing Guidelines

Opening the Box

The box contains the TeSys Tera modules and their respective accessories which are shown in the below image.

  1. Modules: LTMT main unit, LTMTCT/LTMTCTV sensor module, LTMT expansion module, LTMTCUF control operator unit, and cables.

  2. Light Instruction Sheet

Modules and Cables

In the Box

LTMT main unit

LTMTCT/LTMTCTV sensor module

The box also contains two screws for mounting the LTMT main unit on top of the sensor module.

LTMT expansion module

LTMTCUF control operator unit

LTMT main unit to LTMTCT/LTMTCTV sensor module RJ11 connector cable

LTMT main unit to LTMT expansion module RJ45 connector cable

LTMT main unit to LTMTCUF control operator unit RJ45 connection cable

Peelable Label Instructions

The peelable label is on the front face of the LTMT main unit.

  1. Read the following instructions printed on the label before removing it:

    WARNING
    UNINTENDED EQUIPMENT OPERATION
    • Ensure the DO contacts of the LTMT main unitare set to the Normally Open (NO) position using a multi meter.
    • Ensure to provide auxiliary power supply to the LTMT main unitbefore applying the motor control voltage.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
    NOTE: Turn ON the power module to set DO in NO condition, when there is no load connected.

  2. The following table represents the normal state for the DO contacts:

    Terminal Details Expected State
    Verify between O3 NO and O3 C2 NO
    Verify between O3 NC and O3 C2 NC
    Verify between O1 13 and C1 14 NO
    Verify between O2 23 and C1 14 NO
    If any of the above mentioned state do not match, power on the relay and verify that the contact outputs correspond to the specified state.

  3. To remove the peelable label, hold the notch provided and peel the label off the LTMT main unit

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?