DOCA0356EN-01

Power Supply Wiring

DC Power Supply

A dedicated 24 Vdc power supply is necessary to supply:

  • One or several LTMT main unit including the digital inputs of the LTMT main units.

  • The digital inputs of the LTMT expansion modules.

An additional specific 24 Vdc power supply is necessary to supply:

  • LTMT main unit digital outputs

  • Other devices

The LTMT main unit DC power supply must have the following characteristics:

  • AC/DC converter

  • Galvanic isolation input AC/output DC: 4 kVac minimum at 50 Hz

  • SMPS input voltage: 100–240 Vac (+15%/-20%)

  • SMPS output voltage: 24 Vdc (+/-10%)

The following Schneider Electric ABL8RPS24••• power supplies are recommended:

Reference number

Input voltage

Output voltage/current

Maximum number of LTMT main units supplied

ABL8RPS24100

100–500 Vac

24 Vdc/10 A

25

ABL8RPS24050

100–500 Vac

24 Vdc/5 A

10

ABL8RPS24030

100–500 Vac

24 Vdc/3 A

5

AC Power Supply

A dedicated AC power supply or uninterruptible power supply (UPS) is necessary to supply:

  • One or several LTMT main unit

  • Digital inputs of the LTMT expansion module

An additional specific AC power supply is necessary to supply:

  • LTMT main unit digital outputs

  • Other devices

The LTMT main unit AC power supply or UPS must have the following characteristics:

  • Isolation transformer

  • Transformer output voltage: 115 or 230 Vac (+15%/-20%)

  • 115 Vac output voltage is recommended

  • Power according to the number of LTMT main unit (several AC supplies are recommended)

  • UPS is recommended if voltage is unstable and does not follow standard EN 50160

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?