DOCA0276EN-02

Introduction

Overview

The TeSys Tera system helps to provide complete protection, control, and monitoring capabilities for single-phase or three-phase AC induction motors. The system is installed in the low voltage switchgear system and connects the higher level automation system through fieldbus network and the motor feeder.

These firmware packages support the following LTMT main units of the TeSys Tera system:

  • LTMTEBD

  • LTMTEFM

  • LTMTMBD

  • LTMTMFM

  • LTMTPFM

  • LTMTPBD

NOTE: Firmware for the LTMTCT/LTMTCTV sensor module and the LTMT expansion modules are updated by the respective LTMT main units.

For more information, refer to TeSys Tera Motor Management System User Guide – DOCA0257EN

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.