TME9377200

Safety Precautions

Read and understand the following precautions before performing any procedures in this guide.

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E or CSA Z462 or local equivalent.
  • This equipment must be installed and serviced only by qualified personnel.
  • Service only after reading and understanding all of the instructions contained in this bulletin.
  • Turn off all power supplying this equipment before working on or inside equipment.
  • Before performing visual inspections, tests, or maintenance on this equipment, disconnect all sources of electric power. Assume all circuits are live until they are de-energized, tested, and tagged. Pay particular attention to the design of the power system. Consider all sources of power, including the possibility of backfeeding.
  • Always use a properly rated voltage sensing device to confirm power is off.
  • Install, operate, and maintain the equipment for it to function properly. Neglecting fundamental installation and maintenance requirements may lead to personal injury, as well as damage to equipment or other property.
  • Inspect installation area and remove any tools and objects left inside the equipment.
  • Replace all devices, doors, and covers before turning on power to this equipment.
  • All instructions in this manual assume that the customer has taken these measures before performing maintenance or testing.
Failure to follow these instructions will result in death or serious injury.

WARNING: This product can expose you to chemicals including Nickel compounds), which are known to the State of California to cause cancer, and Bisphenol A (BPA), which is known to the State of California to cause birth defects or other reproductive harm. For more information go to www.P65Warnings.ca.gov.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?