TME9377200

Voltage Transformers

Inside the utility compartment a mounting pan is provided for the installation of up to four voltage transformers.

Wires of the CTs and VTs can be routed out of the utility compartment by using any of the two knockouts provided, one located on the mounting pan for voltage transformers, and the other located on the sidewall.

Knockouts and VT Installation on the Utility Compartment

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?