Auxiliary Contact

There are two categories of auxiliary contacts respectively for TransferPacT Active Automatic / Automatic transfer switching equipment.

The table provides the list of auxiliary contacts:

Switch

Type of auxiliary contact

Auxiliary contact

Frame 100: 32–100 A

Source Position

TPSAUX32

OFF Position

TPSAUX33

Frame 160: 80–160 A

Source Position

TPSAUX32

OFF Position

TPSAUX33

Frame 250 100–250 A

Source Position

TPSAUX43

OFF Position

TPSAUX44

Frame 630: 320–630 A

Frame 800: 800 A

Source Position

TPSAUX43

OFF Position

TPSAUX44

Frame 1A: 800–1600 A

Source Position

TPSAUX71

OFF Position

TPSAUX72

For information on installation, consult the instruction sheets on Schneider Electric website:

  • TransferPacT Active Automatic / Automatic 32-100 A: JYT3049801

  • TransferPacT Active Automatic / Automatic 80-160 A: JYT3049901

  • TransferPacT Active Automatic / Automatic / Remote 100–250 A: GEX2525501

  • TransferPacT Active Automatic / Automatic / Remote 320–630 A: GEX2525601

  • TransferPacT Active Automatic / Automatic / Remote 800 A: BQT1751501

  • TransferPacT Active Automatic 800–1600 A: BQT7680301

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?