Active Automatic HMI with LCD Display

The Active Automatic HMI with LCD display of the switch matches to all extension accessories using TPCDIO15. It displays all logs and settings with password protection. It can also be extended with more advanced functions, such as communications with extension plus 24 V DC.

Active Automatic HMI Settings

Label

Description

Function

1

LCD screen

LCD screen for display

2

ESC

ESC button to cancel the selected option or return to the previous menu

3

Up button

Up navigation button for rolling up

4

Down button

Down navigation button for rolling down

5

OK button

OK button to confirm the selected option

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?