Load Shedding and Availability Warning

The load shedding and availability warning is an accessory module installed on TransferPacT Automatic and TransferPacT Active Automatic controller with following functions:

  • Load shedding output, 1 NO and 1 NC dry contacts is provided.

  • Available warning, 1 NO dry contact is provided.

  • Green LED is on the top of the accessory indicates the power status and proper connection of the accessory.

  • Communication with the main MCU on ATSE.

  • Only one load shedding and availability warning is allowed to be installed on one product.

Application Load Shedding

The alternate power (genset) sometimes may not afford all loads. A signal from controller will shed some non-critical loads.

Load shedding will send the signal after enabling this function.

Application Availability Warning

When transfer switch is not in auto or power lost on two sources, a dry contact will give the signal.

After back to auto status or power recovery, the signal will be stopped.

Terminals

Load shedding: 1 NO + 1 NC

  • NO: LS1-LS4

  • NC: LS1-LS2

When load shedding initiates, NC terminal will open, and NO terminal will close.

For status output: 1 NO

  • NO: AW1-AW2

When availability warning initiates, NO terminal will close.

Signal Type

Digital output.

Performance

Electrical characteristics

Ratings

Ui

300 V

Maximum output voltage

250 VAC, 50 / 60 Hz or 30 VDC

Maximum output current

5 A

Over voltage category

III

Pollution degree

3

Altitude

2000 m

Cable Capacity for Terminals

The cable capacity for the terminals are 0.05 – 2.6 mm2 (AWG 30 ~ 13).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?