Local Control Mode

CAUTION
HAZARD OF EQUIPMENT DAMAGE
Enable the local control through Active Automatic HMI to exit the auto mode.
Failure to follow these instructions can result in injury or equipment damage.
NOTICE
Potential Power outage OF EQUIPMENT
To re-enter Auto mode, disable local control through Active Automatic HMI or External HMI.
Failure to follow these instructions can result in equipment damage.

The local mode is activated through the HMI (only available for Active Automatic HMI). It allows locally to change the logical position of the TSE. The switch will refuse to active if the action will damage the driving system. It cannot transfer to unavailable source.

NOTE: Local transfer will not be active, if transfer action damage driving system (for example, both sources are out of range, TSE refuses to transfer) or both sources are out of operating voltage of solenoid.

Auto Genset start signal and load shedding signal is not available for this mode. In this case, the target source conformity is verified before transfer and time delays are not considered.

Local Control to N

The command is sent through HMI. There is no time delay except OFF delay.

The switch will transfer to normal after receiving the order to it when normal power is in tolerance.

Local Control to A

The command is sent through HMI. There is no time delay except OFF delay.

The switch will transfer to alternate after receiving the order to it when alternate power is in tolerance.

Local Control to O

The command is send through HMI. There shall be no time delay. The switch will transfer to OFF after receiving the order to it.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?