Modbus RTU (Serial Port)

The modbus is an accessory module installed on TransferPacT Active Automatic controller with following functions:

  • Modbus RTU communication supporting MODBUS protocol.

  • Indicate the com status of the accessory by using a yellow LED on top of the accessory.

  • Green LED on the front face of the accessory indicates the power status and proper connection of the accessory.

  • Communication with the main MCU on ATSE.

  • Support communication transfer.

  • Two Modbus are allowed to be installed on one product.

Application Modbus

Modbus can be used to connect with other system. It require external 24 V or at least one main source to keep the communication with protocol Modbus RTU.

For a cable length up to 300 m (1.000 ft), it is mandatory to use a shielded twisted cable. The shield of cable is connected to the shield terminal.

Terminals Modbus

  • Modbus:

    • D1, D0, 0V, Shield

Signal Type

Serial port.

Performance

Electrical Characteristics

Ratings

Ui

30 V DC

Baud Rate (KBS)

4.8 / 9.6 / 19.2

Over voltage category

III

Pollution degree

3

Altitude

2000 m

Cable Capacity for Terminals

The cable capacity for the terminals are 0.05 – 2.6 mm2 (AWG 30 ~ 13).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?