External HMI

The External HMI is used to display the settings parameters remotely. It displays the same parameters as shown on ATSE and has higher priority. There are two parts of External HMI:

  1. External HMI base, which is mounted on the panel doors.

  2. LCD screen with embedded HMI.

NOTE: The function module TPCDIO15 and HMI cable with RJ45 port is needed to connect the external HMI.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?