Threshold

Description

Settings

Default setting  
% of nominal

Adjustment range
increments of 1%

Note

Normal source voltage

Under voltage Dropout

85%

70%-95%

Step of 1%

Under voltage Pickup

90%

85%-100%

Step of 1%

Over voltage Dropout

110%

105%-135%

Step of 1%

Over voltage Pickup

105%

100%-115%

Step of 1%

Minimum differential between Dropout and pickup

2%

--

 

Alternate source voltage

Under voltage Dropout

85%

70%-95%

Step of 1%

Under voltage Pickup

90%

85%-100%

Step of 1%

Over voltage Dropout

110%

105%-135%

Step of 1%

Over voltage Pickup

105%

100%-115%

Step of 1%

Minimum differential between Dropout and pickup

2%

--

 

Normal source frequency

Under Frequency Dropout

96%

80%-98%

Step of 0.5%

Under Frequency Pickup

97%

85%-100%

Step of 0.5%

Over Frequency Dropout

102%

101%-120%

Step of 0.5%

Over Frequency Pickup

101%

100%-115%

Step of 0.5%

Minimum differential between Dropout and pickup

0.50%

--

 

Alternate source frequency

Under Frequency Dropout

96%

80%-98%

Step of 0.5%

Under Frequency Pickup

97%

85%-100%

Step of 0.5%

Over Frequency Dropout

102%

101%-120%

Step of 0.5%

Over Frequency Pickup

101%

100%-115%

Step of 0.5%

Minimum differential between Dropout and pickup

0.50%

--

 

Voltage unbalance

 

Default as disabled

2%-30%

 

Phase rotation

 

enabled

 

 

Neutral wrong connection

 

enabled

 

 

Neutral lost

 

disabled

 

unbalance rate

The accuracy of voltage sensing is 1%.

The accuracy of frequency sensing is 0.1%.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?