DUG_Smoke Alarm AC_LK-00

Removing the device from the Wiser app

You can remove a device from the device list using the Wiser app,
  1. On the Home page, tap All devices > Smoke Alarm.
  2. Tap to display more details.
  3. Tap Remove and Factory Reset Device (A) and tap Confirm.

    TIP: Alternatively, you can tap and hold on theSmoke Alarm on the Home page to remove the device.
    NOTE: By removing the device, you will reset the device. If you still have a problem with the reset, then refer to resetting the device.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?