DUG_Smoke Alarm AC_LK-00

Test alarm reminder

You can set a reminder for the test alarm in the Wiser app.
  1. On the Home page, tap All devices > Smoke Alarm.
  2. On the device control panel page, tap Settings.
  3. Tap the Test Alarm Reminder toggle switch (A) to turn on the reminder.


NOTE: If the test alarm reminder is enabled, the app sends a monthly reminder to perform a test alarm on the first day of every month.
The reminder is also stored in the Notification history under Messages.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?