DUG_Smoke Alarm AC_LK-00

Setting LED brightness

You can change the LED brightness to minimum and maximum manually or by using Wiser app.

Changing the LED brightness manually

  1. When the device is in standby mode, short press the test/hush button 3 times within 2 s.

  2. When the Red LED is On, short press the Test/Hush button to switch between Min. and Max. LED brightness.

  3. Again short press the Test/Hush button 3 times within 2 s to store the adjusted brightness level. Otherwise, you can wait 30s for the standby LED to turn off, then the brightness level will be saved.

Changing the LED brightness using app

  1. On the Home page, tap All devices > Smoke Alarm.

  2. On the device control panel page, tap Settings.

  3. Tap on LED Indicator Light Level (A).

  4. Follow the settings mentioned in the pop-up notification, then tap Ok (B).

  5. Select Min or Max indicator level (C).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?