DUG_Window door sensor_LK-00

For your safety

NOTICE
EQUIPMENT DAMAGE
  • Do not install the sensor near magnetic devices to avoid degrading its performance.
  • With a window/door in the closed state, the distance between the primary and secondary parts of the sensor should be <18 mm for a non-metallic base (for example, wood or plastic surfaces) and <10 mm for a metallic base.
Failure to follow these instructions can result in equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?