DUG_Window door sensor_LK-00

About the device

The Wiser Window/Door Sensor (hereinafter referred to as sensor) consists of two separate parts: Primary and Secondary. The primary part includes the sensing circuit which detects the secondary part. The secondary part is a magnet.

When the sensor is connected to the Wiser Gateway and the window/door is opened or closed, the primary part directly reports the change to the app via Wiser Gateway.

Operating elements

  1. Primary part (sensing circuit)

  2. Secondary part (magnet)

  3. Status LED

  4. Function key

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?