DUG_Water leakage sensor_WSE-02

For your safety

NOTICE
EQUIPMENT DAMAGE
  • Avoid locations where the sensor may be accidentally kicked or otherwise moved. The best locations are on the floor in corners, within cabinets with exposed plumbing, beneath cabinets, or other fixtures.
  • Do not locate the sensor right beneath the place where leakage is likely to happen.
  • Do not locate the sensor at the area with rain, oil smoke and steam of cooking range.
  • Do not install the sensor in a location with contaminated water such as oil or frozen water such as ice or snow.
  • Do not completely immerse the sensor into the water.
Failure to follow these instructions can result in equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?