DUG_Water leakage sensor_WSE-02

Example of an automation

This demonstration shows you how to create an automation to get notification on your app when the water leakage is detected.
  1. Go to Automation > + to create an automation.
  2. Tap Edit name, enter the name of the automation and tap Save.
    TIP: You can choose the cover image that best represents your automation by tapping .
  3. Tap Add Condition > When device status changes > Water Leakage Sensor.
  4. Tap Water detection state > Detected and tap Next.
  5. Tap Add task > Send notification and select Notifications (A).
  6. Tap Next.

  7. In the Automation Settings page, tap Save.

    Once the automation is saved, it is visible on the Automation tab. You can tap the toggle switch on the automation to enable it.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?