DUG_Water leakage sensor_WSE-02

Replacing the batteries

To replace the batteries:
  1. Use a screwdriver to remove the six screws from the battery cover to access the batteries.
  2. Make sure you replace the batteries with the correct polarity.
  3. Secure the battery cover and tighten the six screws using a screwdriver.
    The LED blinks green seven times and then stops blinking.
    IMPORTANT: Dispose used batteries, as per statutory regulations.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?