DUG_Window/Door Sensor_WSE-02

Using the Device

The Control Panel of the Sensor allows you to view if the window/door is opened or closed.

On the Home page, tap All devices > Window/Door Sensor to access the control panel.

On the Sensor control panel page, you can see the following:

  • Battery level (A)

  • Window/Door status (B)

  • History (C)


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?