DUG_Window/Door Sensor_WSE-02

Pairing device with auto scan

Pairing the device with auto scan automatically discovers the device when it is powered on.
To pair the device:
  1. On the Home page, tap +.
  2. Tap Auto scan and than tap Confirm.
  3. If you have multiple hubs, do Step 4 or proceed to Step 5.
  4. Tap Select hub and select the Wiser hub from the slide-up menu.
  5. Short press the function key 3 times (< 0,5 s).
    NOTE:
    • The LED blinks orange.

    • Wait for a few seconds until the device is detected.

  6. If more than one device is in pairing mode, select the required device and tap Next (A).

  7. Once the device is added successfully, tap Done.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?