DUG_Exxact Connected Motion Sensor with Push-button Dimmer LED_WH-01

About the device

The Connected Motion Sensor with Push-button Dimmer LED (hereinafter referred to as Motion Sensor Dimmer) detects moving heat sources (e.g. persons) and can dim ohmic, inductive or capacitive loads and switch them on for a settable overtravel time.

Control options

Home control: To control the motion sensor through the Wiser Home app you will need the Wiser Hub.

Direct operation: The motion sensor can always be controlled directly on-site. You can also connect any number of mechanical push-buttons to control the device.

Functions

  • Automatic load detection.

  • Thermal protection, overload-resistant, short-circuit protection, soft start, soft stop.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?