DUG_Exxact Connected Motion Sensor with Push-button Dimmer LED_WH-01

Amazon Alexa™

Amazon Alexa™ (Alexa) is an intelligent personal assistant developed by Amazon™, and is capable of voice interaction.

Common Wiser commands for Alexa

  • Inquiry: “Alexa, is the Motion Sensor Dimmer On?”

  • Motion detection: “Alexa, is the sensor detecting movements?”

  • Turn the device on/off: “Alexa, turn on/off the Motion Sensor Dimmer”.

  • Brightness level %: “Alexa, increase or decrease the brightness by XX percentage”.

  • Minimum brightness: “Alexa, set the Motion Sensor Dimmer to minimum brightness”.

  • Maximum brightness: “Alexa, set the Motion Sensor Dimmer to maximum brightness”.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?