DUG_Exxact Connected Motion Sensor with Push-button Dimmer LED_WH-01

Adjusting the brightness level using app

  1. On the Control tab, tap All devices or the room tab where the Motion Sensor Dimmer is located.
  2. On the Device Control Screen, drag the slider bar up/down to increase/decrease the brightness (A).
    TIP: You can also turn on/off the device on the Device Control Screen, tap (B) to turn on/off the Motion Sensor Dimmer.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?