DUG_Exxact Multiwire Push-button Dimmer_WH-02

Configuring the device

The Device Details screen allows you to configure the device settings according to your preferences.
  1. On the Home screen, tap .

  2. Tap Devices > Lights > Dimmer to locate to the Device Details screen.

    NOTE: You can also navigate by tapping Control > Select the device > > Device Settings.

A

Device Name: Tap to change the name of the device.

B

Location: Tap to assign the dimmer to any room (such as living room, bedroom, kitchen etc). For more information, refer to Setting the device location.

C

RL-LED Mode: You can improve the dimming quality in the app if you have problems with light flickering. Tap the toggle switch to enable the RL-LED Mode.

TIP: Fore more information, refer toTechnical Data.

D

LED Indicator Behaviour: Tap to set the LED indicator behaviour of the dimmer as per your preference. Refer to Setting up the LED Indicator Behaviour for detailed information on each options.

E

Power On Behaviour: Tap to set the default brightness level of the dimmer when it is turned on. Refer to Setting up the Power On Behaviour for detailed information on each options.

F

Minimum Brightness and Maximum Brightness: This setting allows you to set limits on the maximum and minimum brightness of the connected load. This is done to avoid flickering and switching off the LED.

Drag the slider bar to increase or decrease the Minimum Brightness and Maximum Brightness.

IMPORTANT: If the light does not begin to brighten up from 0%, adjust the minimum level setpoint to the point where the light actually starts to brighten. Similarly, for maximum brightness, set the maximum level based on the behaviour of the connected light. For example, if brightness does not increase between 80% and 100%, then set the maximum level to 80%.
NOTE: The minimum brightness must be lower than the maximum brightness.

G

Neutral wire fitted?: You can check if the neutral wire is connected during the device installation.

The Wiser Home app automatically detects the wiring mode based on the installation, eliminating the need for manual selection.

  • Yes: Installed with a neutral wire.

  • No: Installed without a neutral wire.

H

Identify: Tap to identify the device. The status LED blinks red and connected lighting devices blinks on/off, upon successful identification of the dimmer.
Tap OK when you finish identifying the device.

I

Delete: Tap to remove the device from the system.

NOTE:
  • Removing the device will also reset the dimmer. After reset, the LED turns amber indicating that the dimmer is ready for pairing.

  • If there is a problem while pairing or resetting the dimmer, refer to Resetting the device.

J

Zigbee Signal Strength Indicator: Zigbee Signal Strength indicator which displays the current signal strength of the device.

  • Good Signal (between 0 & -54dBm)

  • Normal Signal (between -54 & -79dBm)

  • Poor Signal (<-79dBm)

  • No Signal (device is offline)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.